Skip to main content
PPiór.1
Associate II
Aug 30, 2021 6:41 PM UTC
Question

STM32 - USB HS device with DMA and Isonchronous Transmission to stm32

As part of my thesis, trying to get as much data transfer from PC to STM32 as possible. As I am going to transfer a video stream, isonchronous transmission seems to be a good choice, but I don't know how to do it properly.

I use STM32H743 microcontroller with USB3300 as external PHY.

What I have done so far is to rewrite the USBD_CDC library to use endpoint out as isoc instead of bulk.

I changed in the endpoint descriptor as follows:

bmAttributes = 0x1
wMaxPacketSize = 0x400
bInterval = 0x1

In addition, in the USBD_LL_OpenEP function, I changed the endpoint type and the packet size similarly to the descriptor.

I'm testing this with pyusb, sending a 1024byte packet 1000 times and it's works bad.

On STM32 I can see incoming packets, but only 20% are arriving

I don't know if this is working as it should. From what I observe, after each packet comes an interrupt USB_OTG_GINTSTS_OEPINT,

in which I have to move the pointer for DMA anyway (by calling USBD_LL_PrepareReceive with recive_buff + new offset)

- that's not how DMA should work, is it?

Additionally I keep getting (I don't know how often but probably every few ms) USB_OTG_GINTSTS_PXFR_INCOMPISOOUT interrupts which I don't know what to do with.

I can see that my previous approach is wrong. How to do it properly? Do you know any cool examples?

I need all your advice.

This topic has been closed for replies.

3 replies

Walid ZRELLI
Visitor II
Sep 21, 2021 11:01 AM UTC

Hello @Piotr Piórkowski​ ,

Your issue has been raised internally. I will keep you informed.

Thank you for your contribution.

BeST regards,

Walid

Walid ZRELLI
Visitor II
Sep 21, 2021 1:11 PM UTC

Hello @Piotr Piórkowski​ 

Actually we provide an audio example for isochronous OUT transfer to stream audio from PC to STM32.

Check the following example and try to adapt it to your use case :

  • Path: Projects\STM32H743I-EVAL\Applications\USB_Device\Audio_Standalone

This could help you.

BeST Regards,

Walid

Walid ZRELLI
Visitor II
Oct 5, 2021 9:30 AM UTC

Hello @Piotr Piórkowski​ ,

Please click on Select as Best if my post fully answered your question. This will help other customers with the same issue to find the solution faster

BeST Regards,

Walid