Skip to main content
STAR
Associate III
Jan 14, 2021 9:00 AM UTC
Question

STM32 USB HID Keyboard implementation with Media key

Hi All,

I wanted to implement functionality for the volume up/ volume down/ mute etc.

I Got the keycodes for those buttons in USB HID Usage table .

volume up = 128

volume down = 129

mute = 127

but it wont works in My USB HID keyboard code

How to implement this functionality

Regards,

STAR

This topic has been closed for replies.

2 replies

Ben K
Senior III
Jan 17, 2021 7:51 PM UTC

You will need https://github.com/IntergatedCircuits/HidReportDef

then use this HID report descriptor:

static const uint8_t DescPlayerReport[] =
{
/* Consumer device as input controller */
HID_USAGE_PAGE_CONSUMER,
 HID_USAGE_CMR_CONSUMER_CTRL,
 HID_COLLECTION_APPLICATION(
 HID_USAGE_MIN_8(0),
 HID_USAGE_MAX_8(0xFF),
 HID_REPORT_SIZE(8),
 HID_REPORT_COUNT(1),
 HID_LOGICAL_MIN_8(0),
 HID_LOGICAL_MAX_8(0xFF),
 HID_INPUT(Data_Arr_Abs),
 ),
};

Then you just need to send one byte messages (e.g. 128 and 0 to simulate press and release of volume up).

Robmar
Senior II
Mar 22, 2025 4:10 AM UTC

For Host keyboard implementation, what's needed to detect volume up/down, as these keys don't seem to generate a keypress, are they read like the shift and alt keys?