Skip to main content
Visitor II
Jul 19, 2025 2:20 PM UTC
Question

STM32 USB CDC not working for F0, F4 boards

I have tried USB examples for Stm32F070, F401, F407 Black board and calling a single "CDC_Transmit_FS" function to print a string but none is working. The hcdc->TxState value is some garbage big value so it always stay busy and also not getting interrupts for USB receive as I have put break points in it too. The STM32 device show up as "composite" instead of VCP.

For configuration it is RCC->Bypass Clk, USB connectivity->Device Only, USB_Device->VCP, heap size->0x1000.

This topic has been closed for replies.

1 reply

ST Technical Moderator
Oct 23, 2025 1:52 PM UTC

Hi @Lakshay 

Would you point me directly to example firmware not working, and full hardware setup including board revision? 

If your device enumerates incorrectly or driver installation is stuck, changing the PID is a workaround to force the OS to reload the USB driver and re-enumerate the device properly.

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL