Skip to main content
Senior
Jun 26, 2025 9:39 AM UTC
Solved

STM32 Touch Sensing issue with ChD->Delta

Greetings! 
I am testing a touch button in a custom board using stm32u585 mcu. 
I try to follow the following workshops available on YouTube: 
Workshop 1 
Workshop 2 

The thing is, I tested in Debug Mode like in Workshop 1 in minute 15 and I could see the Delta value changing. Since the thing was working I try to implement the touch in my project. The thing is, now Delta is staying fixed, and I have absolutely no idea why it is happening. I can see the p_Data->StateId changing (PROX, DETECT, etc) but Delta value is the same. Any clue where I could be having the problem? I did not do the "MyTKeys[0].p_ChD->Delta /= 3;" in tsl_user.c, nor in the first test, and it worked at the first time.

So basically my code in main.c was something like this: 

 

#include "tsl.h"
#include "touchsensing.h" 

... 

int main(void)
{ 
 "ALL THE INITS"
 tsl_user_Init();
 
 tsl_user_status_t status; 
 
 while(1)
 {
	 tsl_status = tsl_user_Exec();
	 if(tsl_status != TSL_USER_STATUS_BUSY)
	 {
		 if(MyTKeys[0].p_Data->StateId == TSL_STATEID_DETECT)
		 {
			 LED_TEST_SET;
		 }
/*		 else if(MyTKeys[0].p_Data->StateId == TSL_STATEID_PROX)
		 {
		 LED_TEST_SET;
		 } */
		 else
		 {
			 LED_TEST_CLR;
		 }

		 switch(tsl_status)
		 {
			case TSL_USER_STATUS_BUSY:
				break;
			case TSL_USER_STATUS_OK_ECS_ON:
				break;
			case TSL_USER_STATUS_OK_NO_ECS:
				break;
			default:
				break;
		 }
	 }
	 HAL_Delay(5);
 }
This topic has been closed for replies.
Stassen.C
Stassen.CBest answer
ST Employee
Jul 21, 2025 9:14 AM UTC

Hello j_filipe ,

The easiest way to use the touch sensing is to take the example from the stmcube package available on st.com

https://www.st.com/en/embedded-software/stm32cubeu5.html#get-software

From the example you can easily setup the sensors.

Regards,
Stassen

 

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

2 replies

Stassen.C
Stassen.CBest answer
ST Employee
Jul 21, 2025 9:14 AM UTC

Hello j_filipe ,

The easiest way to use the touch sensing is to take the example from the stmcube package available on st.com

https://www.st.com/en/embedded-software/stm32cubeu5.html#get-software

From the example you can easily setup the sensors.

Regards,
Stassen

 

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
j_filipeAuthor
Senior
Jul 28, 2025 9:49 AM UTC

Thank you Stassen,
I figured it out, I must have erased some code unintentionally, I started from scratched and it worked again.
Cheers!