Skip to main content
JBurg.5
Associate II
Feb 5, 2025 9:03 AM UTC
Question

STM32 SDIO SD card initialization

Hi,

I have an STM32F7 design with SD card connected via SDIO interface.

In many posts I read that SD cards have to be initialized with a 1 bit wide bus and a clock of 400 kHz. Switching the bus width from 1 to 4 bit using the command HAL_SD_ConfigWideBusOperation(&hsd1, SDMMC_BUS_WIDE_4B) is simple. However, I have some doubts about the clock frequency. Many examples inizialize the clock at higher frequencies in the first initialization. This seems to contradict the SD card specification.

Best regards

Jan

This topic has been closed for replies.

1 reply

I.KHACHINE
ST Employee
May 20, 2025 3:06 PM UTC

Hi JBurg.5,

In our SD driver, in initialization API, we are forcing the card initialization to use 1bit @400Khz, then switching the user settings configured in init structure. I confirm that the Initialization is compliant with the SD Standard.
I hope that is clear now.

Best Regards,
Ismail