Skip to main content
gsaru.1
Associate II
Apr 26, 2022 3:48 PM UTC
Question

STM32+FreeRTOS issue when using "HAL_UART_TRANSMIT_IT"

Hello,

We want our device (STM32-F446RE running FreeRTOS + Telit ME310G1 modem) to communicate to the AWS cloud. We are trying to follow the Cellular Interface Library Demo, in particular following the diagram- https://www.freertos.org/fr-content-src/uploads/2020/12/cellular_demo_sequence-1.png

We are using coreMQTT Agent, MbedTLS libraries, the following communication interface (UART)- https://github.com/aws/amazon-freertos/blob/feature/cellular/vendors/st/boards/stm32l475_discovery/ports/comm_if/comm_if_uart.c

And this UART API implementation- https://github.com/aws/amazon-freertos/blob/feature/cellular/vendors/st/boards/stm32l475_discovery/ports/common_io/iot_uart.c

UART using 115200 baud rate.

Currently failing on the Cellular_Init function when trying to send the first AT command to the modem, specifically when calling the HAL_UART_TRANSMIT_IT function from the above comm interface send function. While debugging we see that the USART1_IRQHandler is called infinite times and nothing is sent through the UART communication.

We are using the default handler, do we need to implement it in any way?

void USART1_IRQHandler(void)
{
 HAL_UART_IRQHandler(&huart1);
}

Any help will be appreciated.

Thanks in advance,

Guy

This topic has been closed for replies.