Skip to main content
Associate
Aug 26, 2024 6:10 AM UTC
Question

STM32 Firmware Upgrade using Pendrive

I need help with STM32F4 Firmware Upgrade Using Pendrive. 

I tried the FW Standalone Upgrade Application given for STM32F429 Discovery Board. But the code is giving hard fault error. It opens the directory properly and opens the file. But when it reaches the read function it gives error when reaches validate function inside f_read() function. I have not been able to debug and understand the exact point of issue. If anyone can provide some inputs will be helpful.

Or else if someone has a working code for the bootloader and can share it will be really appreciated.

Thankyou. 

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
Aug 26, 2024 6:34 AM UTC

Instrument better so you understand what is happening. Determine exact point of Hard Fault and the registers and assembler code that causes it.

Instrument at the DISKIO level.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
BhavikSAuthor
Associate
Aug 26, 2024 6:42 AM UTC

I have tried this but I am not able to understand the exact reason yet. I have been able to trace it upto this point : it goes to f_read -> validate() -> disk_status -> stat = disk.drv[pdrv]->disk_status(disk.lun[pdrv]); This is the line where I get the hard fault error. If tried to check where these variables are set but could not find in the code. If u can guide me further wrt what might have gone wrong?