Question
stm32 f107 i2s and sd card via dma
void DMA1_Channel5_IRQHandler()
{
if(DMA_GetFlagStatus(DMA1_FLAG_TC5))
{
transfer_complete_flag=1;
DMA_ClearFlag(DMA1_FLAG_TC5);
}
if(DMA_GetFlagStatus(DMA1_FLAG_HT5))
{
ht_c=1;
DMA_ClearFlag(DMA1_FLAG_HT5);
}
}
int counter=0;
int sd_ok=0;
int main()
{
int loop=0;
GPIO_INIT();
USART1_INIT();
SPI_INIT();
Debug_Port(" uart ready debugging..... \r\n");
I2S_GPIO_Config();
I2S_Config();
DMA_setup();
if(f_mount(&FatFs, "", 1) == FR_OK)
{
Debug_Port("SD card Mounted SuccessFully!!!\r\n");
if(f_open(&fil,"m_16.wav", FA_OPEN_EXISTING | FA_READ) == FR_OK)
{
f_read(&fil,&music_buffer,100,&bw);
WaveFileStatus=WavePlayer_WaveParsing(&wavelen);
// if (WaveFileStatus == Valid_WAVE_File) /* the .WAV file is valid */
// {
/* Set WaveDataLenght to the Speech wave length */
WaveDataLength = WAVE_Format.DataSize;
// }
//f_close(&fil); // close the file
Debug_Port("file read complete\r\n"); // print the output at Debug Window
}
f_lseek(&fil, WaveCounter);
f_read (&fil,music_buffer,2000,&bw);
DMA_InitStructure.DMA_MemoryBaseAddr =(uint32_t)&music_buffer;
DMA_InitStructure.DMA_BufferSize =2000;
DMA_Init(DMA1_Channel5, &DMA_InitStructure);
DMA_Cmd(DMA1_Channel5, ENABLE);
switch_flag=0;
while(dummy_flag==1)
{
if(ht_c==1)
{
ht_c=0;
f_read (&fil,music_buffer,1000,&bw);
}
if(transfer_complete_flag==1)
{
transfer_complete_flag=0;
f_read (&fil,music_buffer_2,1000,&bw);
for(loop=1000;loop<2000;loop++)
{
music_buffer[loop]=music_buffer_2[loop];
}
}
}
}
else
{
Debug_Port("SD card Not Mounted\r\n");
}
while(1)
{
}
}i have interfaced sd card (FATFS) and i2s and also enabled dma to play wave files.i have to play large wave files >5mb how will i do that ? i am able play small files correctly <50 kb files correctly?please help