Skip to main content
Associate
October 24, 2025
Solved

STM32 CAN Bus skips some messages

  • October 24, 2025
  • 4 replies
  • 373 views

Hi, I am using three STM32 devices for CAN communication:

Hardware

  • Device A: STM32G431 (FDCAN)

  • Device B: STM32F303 (Classic CAN)

  • Device C: STM32H7A3 (FDCAN)

Setup

  • A sends a continuous sequence of commands to B.

  • B processes each command and replies to A over the same CAN bus.

  • One specific command requires B to perform a synchronization sequence with C (also over CAN).

  • While B is synchronizing with C, A continues to send commands to B.

Issue

  • During the B↔C synchronization, B intermittently misses some frames from A (i.e., A transmits, but B does not process/see a corresponding message).

  • The failure is not immediate: A↔B + B↔C run together fine for a while (sometimes short, sometimes long), then a frame from A is skipped.

  • When the synchronization with C is disabled, A↔B runs reliably with no missed frames.


CAN ID from A to B: 0x12C
CAN ID from B to A: 0x12D
CAN IDs between B and C (sync purposes): 0x2BC, 0x2BD and 0x2BE

As you can see from the inserted can config the sampling point for 3 devices is at 87.5%. Bitrate is 500000 bps for three of them. 

The CAN configurations for device A:

static void MX_FDCAN1_Init(void)
{

 /* USER CODE BEGIN FDCAN1_Init 0 */

 /* USER CODE END FDCAN1_Init 0 */

 /* USER CODE BEGIN FDCAN1_Init 1 */

 /* USER CODE END FDCAN1_Init 1 */
 hfdcan1.Instance = FDCAN1;
 hfdcan1.Init.ClockDivider = FDCAN_CLOCK_DIV1;
 hfdcan1.Init.FrameFormat = FDCAN_FRAME_FD_NO_BRS;
 hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;
 hfdcan1.Init.AutoRetransmission = ENABLE;
 hfdcan1.Init.TransmitPause = DISABLE;
 hfdcan1.Init.ProtocolException = DISABLE;
 hfdcan1.Init.NominalPrescaler = 40;
 hfdcan1.Init.NominalSyncJumpWidth = 1;
 hfdcan1.Init.NominalTimeSeg1 = 6;
 hfdcan1.Init.NominalTimeSeg2 = 1;
 hfdcan1.Init.DataPrescaler = 25;
 hfdcan1.Init.DataSyncJumpWidth = 1;
 hfdcan1.Init.DataTimeSeg1 = 6;
 hfdcan1.Init.DataTimeSeg2 = 1;
 hfdcan1.Init.StdFiltersNbr = 8;
 hfdcan1.Init.ExtFiltersNbr = 0;
 hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
 if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN FDCAN1_Init 2 */
 FDCAN_FilterTypeDef sFilterConfig;

 sFilterConfig.IdType = FDCAN_STANDARD_ID;
 sFilterConfig.FilterIndex = 0;
 sFilterConfig.FilterType = FDCAN_FILTER_RANGE;
 sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
 sFilterConfig.FilterID1 = 0x12C; 
 sFilterConfig.FilterID2 = 0x18F;
 if (HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig) != HAL_OK)
 Error_Handler();
 
 sFilterConfig.IdType = FDCAN_STANDARD_ID;
 sFilterConfig.FilterIndex = 1;
 sFilterConfig.FilterType = FDCAN_FILTER_RANGE;
 sFilterConfig.FilterConfig = FDCAN_FILTER_REJECT;
 sFilterConfig.FilterID1 = 0x00; 
 sFilterConfig.FilterID2 = 0x12B;
 if (HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig) != HAL_OK)
 Error_Handler();
 
 sFilterConfig.IdType = FDCAN_STANDARD_ID;
 sFilterConfig.FilterIndex = 2;
 sFilterConfig.FilterType = FDCAN_FILTER_RANGE;
 sFilterConfig.FilterConfig = FDCAN_FILTER_REJECT;
 sFilterConfig.FilterID1 = 0x190; 
 sFilterConfig.FilterID2 = 0x31F;
 if (HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig) != HAL_OK)
 Error_Handler();
 /* USER CODE END FDCAN1_Init 2 */

}

 Device B:

static void MX_CAN_Init(void)
{

 /* USER CODE BEGIN CAN_Init 0 */

 /* USER CODE END CAN_Init 0 */

 /* USER CODE BEGIN CAN_Init 1 */

 /* USER CODE END CAN_Init 1 */
 hcan.Instance = CAN;
 hcan.Init.Prescaler = 9;
 hcan.Init.Mode = CAN_MODE_NORMAL;
 hcan.Init.SyncJumpWidth = CAN_SJW_1TQ;
 hcan.Init.TimeSeg1 = CAN_BS1_6TQ;
 hcan.Init.TimeSeg2 = CAN_BS2_1TQ;
 hcan.Init.TimeTriggeredMode = DISABLE;
 hcan.Init.AutoBusOff = DISABLE;
 hcan.Init.AutoWakeUp = DISABLE;
 hcan.Init.AutoRetransmission = ENABLE;
 hcan.Init.ReceiveFifoLocked = DISABLE;
 hcan.Init.TransmitFifoPriority = DISABLE;
 if (HAL_CAN_Init(&hcan) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN CAN_Init 2 */
 CAN_FilterTypeDef canfilterconfig;

 canfilterconfig.FilterActivation = CAN_FILTER_ENABLE;
 canfilterconfig.FilterBank = 0; // which filter bank to use from the assigned ones
 canfilterconfig.FilterFIFOAssignment = CAN_FILTER_FIFO0;
 canfilterconfig.FilterIdHigh = 0x12C<<5;
 canfilterconfig.FilterIdLow = 0;
 canfilterconfig.FilterMaskIdHigh = 0x7FF<<5;
 canfilterconfig.FilterMaskIdLow = 0x0000;
 canfilterconfig.FilterMode = CAN_FILTERMODE_IDMASK;
 canfilterconfig.FilterScale = CAN_FILTERSCALE_32BIT;

 HAL_CAN_ConfigFilter(&hcan, &canfilterconfig);
 
 canfilterconfig.FilterActivation = CAN_FILTER_ENABLE;
 canfilterconfig.FilterBank = 1; // which filter bank to use from the assigned ones
 canfilterconfig.FilterFIFOAssignment = CAN_FILTER_FIFO1;
 canfilterconfig.FilterIdHigh = 0x2BD<<5;
 canfilterconfig.FilterIdLow = 0;
 canfilterconfig.FilterMaskIdHigh = 0x7FF<<5;
 canfilterconfig.FilterMaskIdLow = 0x0000;
 canfilterconfig.FilterMode = CAN_FILTERMODE_IDMASK;
 canfilterconfig.FilterScale = CAN_FILTERSCALE_32BIT;

 HAL_CAN_ConfigFilter(&hcan, &canfilterconfig);
 
 /* USER CODE END CAN_Init 2 */

}

Device C:

void MX_FDCAN1_Init(void)
{

 /* USER CODE BEGIN FDCAN1_Init 0 */

 /* USER CODE END FDCAN1_Init 0 */

 /* USER CODE BEGIN FDCAN1_Init 1 */

 /* USER CODE END FDCAN1_Init 1 */
 hfdcan1.Instance = FDCAN1;
 hfdcan1.Init.FrameFormat = FDCAN_FRAME_FD_NO_BRS;
 hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;
 hfdcan1.Init.AutoRetransmission = ENABLE;
 hfdcan1.Init.TransmitPause = DISABLE;
 hfdcan1.Init.ProtocolException = DISABLE;
 hfdcan1.Init.NominalPrescaler = 12;
 hfdcan1.Init.NominalSyncJumpWidth = 1;
 hfdcan1.Init.NominalTimeSeg1 = 6;
 hfdcan1.Init.NominalTimeSeg2 = 1;
 hfdcan1.Init.DataPrescaler = 12;
 hfdcan1.Init.DataSyncJumpWidth = 1;
 hfdcan1.Init.DataTimeSeg1 = 6;
 hfdcan1.Init.DataTimeSeg2 = 1;
 hfdcan1.Init.MessageRAMOffset = 0;
 hfdcan1.Init.StdFiltersNbr = 8;
 hfdcan1.Init.ExtFiltersNbr = 0;
 hfdcan1.Init.RxFifo0ElmtsNbr = 4;
 hfdcan1.Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_64;
 hfdcan1.Init.RxFifo1ElmtsNbr = 0;
 hfdcan1.Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_8;
 hfdcan1.Init.RxBuffersNbr = 0;
 hfdcan1.Init.RxBufferSize = FDCAN_DATA_BYTES_8;
 hfdcan1.Init.TxEventsNbr = 0;
 hfdcan1.Init.TxBuffersNbr = 0;
 hfdcan1.Init.TxFifoQueueElmtsNbr = 1;
 hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
 hfdcan1.Init.TxElmtSize = FDCAN_DATA_BYTES_64;
 if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN FDCAN1_Init 2 */
 FDCAN_FilterTypeDef sFilterConfig;

 sFilterConfig.IdType = FDCAN_STANDARD_ID;
 sFilterConfig.FilterIndex = 0;
 sFilterConfig.FilterType = FDCAN_FILTER_RANGE;
 sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
 sFilterConfig.FilterID1 = 0x01; 
 sFilterConfig.FilterID2 = 0x12B;
 if (HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig) != HAL_OK)
 Error_Handler();
 
 sFilterConfig.IdType = FDCAN_STANDARD_ID;
 sFilterConfig.FilterIndex = 1;
 sFilterConfig.FilterType = FDCAN_FILTER_RANGE;
 sFilterConfig.FilterConfig = FDCAN_FILTER_REJECT;
 sFilterConfig.FilterID1 = 0x12C; 
 sFilterConfig.FilterID2 = 0x18F;
 if (HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig) != HAL_OK)
 Error_Handler();
 
 sFilterConfig.IdType = FDCAN_STANDARD_ID;
 sFilterConfig.FilterIndex = 2;
 sFilterConfig.FilterType = FDCAN_FILTER_RANGE;
 sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
 sFilterConfig.FilterID1 = 0x190; 
 sFilterConfig.FilterID2 = 0x1F3;
 if (HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig) != HAL_OK)
 Error_Handler();
 
 sFilterConfig.IdType = FDCAN_STANDARD_ID;
 sFilterConfig.FilterIndex = 3;
 sFilterConfig.FilterType = FDCAN_FILTER_RANGE;
 sFilterConfig.FilterConfig = FDCAN_FILTER_REJECT;
 sFilterConfig.FilterID1 = 0x1F4; 
 sFilterConfig.FilterID2 = 0x257;
 if (HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig) != HAL_OK)
 Error_Handler();
 
 sFilterConfig.IdType = FDCAN_STANDARD_ID;
 sFilterConfig.FilterIndex = 4;
 sFilterConfig.FilterType = FDCAN_FILTER_RANGE;
 sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
 sFilterConfig.FilterID1 = 0x258; 
 sFilterConfig.FilterID2 = 0x351;
 if (HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig) != HAL_OK)
 Error_Handler();
 /* USER CODE END FDCAN1_Init 2 */

}

For sending and receiving CAN messages, the functions are as follows:
Device A:

void HAL_FDCAN_RxFifo0Callback(FDCAN_HandleTypeDef *hfdcan, uint32_t RxFifo0ITs)
{
 CanFrameBuffer *frame = &canRxBuffer[canRxWriteIdx];
 memset(frame, 0, sizeof(CanFrameBuffer));

 if (HAL_FDCAN_GetRxMessage(hfdcan, FDCAN_RX_FIFO0, &RxHeader, frame->data) != HAL_OK)
 {
 Error_Handler();
 }

 canRxWriteIdx++;
 if (canRxWriteIdx >= CAN_RX_BUF_SIZE)
 canRxWriteIdx = 0;
}

void ProcessUSBData(uint8_t *Buf, uint16_t Len)
{
 uint16_t bytesSent = 0;

 while (bytesSent < Len)
 {
 uint8_t chunk[CAN_PAYLOAD_SIZE] = {0};
 uint8_t chunkSize = (Len - bytesSent) > CAN_PAYLOAD_SIZE ?
 CAN_PAYLOAD_SIZE : (Len - bytesSent);
 
 TxHeader.DataLength = dlc_from_len(chunkSize);

 while (HAL_FDCAN_GetTxFifoFreeLevel(&hfdcan1) == 0);
 if (HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1, &TxHeader, &Buf[bytesSent]) != HAL_OK)
 Error_Handler();
 bytesSent += chunkSize;
 }

 // Always send an explicit 0x00 terminator frame
 uint8_t terminator = 0x00;
 TxHeader.DataLength = FDCAN_DLC_BYTES_1;
 while (HAL_FDCAN_GetTxFifoFreeLevel(&hfdcan1) == 0);
 if (HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1, &TxHeader, &terminator) != HAL_OK)
 Error_Handler();
}


Device B. I use two Fifos:
Fifo0: messages from A
Fifo1: messages from C

void HAL_CAN_RxFifo0FullCallback(CAN_HandleTypeDef *hcan)
{
 while (HAL_CAN_GetRxFifoFillLevel(hcan, CAN_RX_FIFO0) > 0) {
 CAN_RxHeaderTypeDef hdr; 
 uint8_t d[8];
 
 if (HAL_CAN_GetRxMessage(hcan, CAN_RX_FIFO0, &hdr, d) != HAL_OK)
 {
 Error_Handler(); // Handle receive error
 }
 
 if (hdr.StdId == Sync_Res) {
 syncAckReceived = 1;
 rx1_sync_isr_count++;
 continue;
 } 
 
 uint8_t next = (uint8_t)((RxWrite + 1u) % RXBUFSIZE);
 if (next == RxRead) {
 // overflow: drop oldest (or set a flag/counter)
 g_swDrops++;
 continue; 
 }
 
 // Use real DLC (0..8) and clear tail
 uint8_t dlc = (uint8_t)(hdr.DLC & 0x0Fu);
 if (dlc > 8) dlc = 8;
 
 RxBuf[RxWrite].id = hdr.StdId; // you’re using standard IDs
 RxBuf[RxWrite].dlc = dlc;
 memcpy(RxBuf[RxWrite].data, d, dlc);
 if (dlc < 8) {
 memset(RxBuf[RxWrite].data + dlc, 0, 8 - dlc);
 }
 
 RxWrite = next;
 }
}

For sending messages:
while (HAL_CAN_GetTxMailboxesFreeLevel(&hcan) == 0);
CAN_SendCommand(cmdID, chunk, idx);

bool CAN_SendCommand(PIPMOD_COMMANDS cmdID, uint8_t *data, uint8_t idx)
{
 TxHeader.DLC = 8; // data length
 TxHeader.IDE = CAN_ID_STD;
 TxHeader.RTR = CAN_RTR_DATA;
 TxHeader.StdId = cmdID; 
 
 if (data == NULL)
 {
 TxHeader.DLC = 0;
 }
 
 if (HAL_CAN_AddTxMessage(&hcan, &TxHeader, (uint8_t *)data, &TxMailbox) != HAL_OK)
 {
 sprintf(responseBuffer, "CAN Transmission failed: %s", GetCommandName(cmdID));
 EnqueueLCErrorResponse(&arCommUnits[idx], UTF8create(responseBuffer, 4), ERROR_INTERFACE_PORTAL);
 return false;
 } 
 
 while (HAL_CAN_IsTxMessagePending(&hcan, TxMailbox));
 return true;
}
void HAL_CAN_RxFifo1MsgPendingCallback(CAN_HandleTypeDef *hcan)
{
 while (HAL_CAN_GetRxFifoFillLevel(hcan, CAN_RX_FIFO1) > 0) {
 CAN_RxHeaderTypeDef hdr; 
 uint8_t data[8]; 

 if (HAL_CAN_GetRxMessage(hcan, CAN_RX_FIFO1, &hdr, data) != HAL_OK) {
 Error_Handler();
 }
 rx1_isr_count++;
 if (hdr.StdId == Sync_Res) {
 syncAckReceived = 1;
 rx1_sync_isr_count++;
 }
 }
}

Device C:

void HAL_FDCAN_RxFifo0Callback(FDCAN_HandleTypeDef *hfdcan, uint32_t RxFifo0ITs)
{
 if (HAL_FDCAN_GetRxMessage(hfdcan, FDCAN_RX_FIFO0, &RxHeader, RxData) != HAL_OK)
 {
 Error_Handler();
 }
 
 if (RxHeader.Identifier == SYNC_START) IsSyncStart = 1;
 if (RxHeader.Identifier == SYNC_END) IsSyncRes = 1; 
}

bool CAN_SendCommand(PORTAL_COMMANDS cmdID, uint8_t *data, uint8_t idx)
{
 if (cmdID == SYNC_RES) { // Device B uses normal CAN (only 8 bytes)
 TxHeader.FDFormat = FDCAN_CLASSIC_CAN;
 TxHeader.DataLength = FDCAN_DLC_BYTES_8;
 }
 else {
 TxHeader.FDFormat = FDCAN_FD_CAN;
 TxHeader.DataLength = FDCAN_DLC_BYTES_64;
 }
 
 if (data == NULL)
 {
 TxHeader.DataLength = FDCAN_DLC_BYTES_0; // no payload
 }
 
 TxHeader.Identifier = cmdID;
 TxHeader.IdType = FDCAN_STANDARD_ID;
 TxHeader.TxFrameType = FDCAN_DATA_FRAME;
 TxHeader.ErrorStateIndicator = FDCAN_ESI_ACTIVE;
 TxHeader.BitRateSwitch = FDCAN_BRS_OFF;
 TxHeader.TxEventFifoControl = FDCAN_NO_TX_EVENTS;
 TxHeader.MessageMarker = 0;
 
 if (HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1, &TxHeader, (uint8_t *)data) != HAL_OK)
 {
 sprintf(responseBuffer, "CAN Transmission failed: %s", GetCommandName(cmdID));
 EnqueueLCErrorResponse(&arCommUnits[idx], UTF8create(responseBuffer, 4), ERROR_INTERFACE_PORTAL);
 return false;
 }
 
 return true;
}

The function for the sync between B and C:
Device B:

bool DoHwSync()
{
 bool finishCmd = false;
 PIPMOD_COMMANDS cmdID1, cmdID2;
 cmdID1 = Sync_Start; //0x2BC
 cmdID2 = Sync_End; //0x2BD
 
 if(IS_FLAG_SET(pipettorState, STATE_WAIT_FOR_SYNC)) 
 {
 
 if(!IsSyncResSent) {
 while (HAL_CAN_GetTxMailboxesFreeLevel(&hcan) == 0);
 if(!CAN_SendCommand(cmdID1, NULL, NULL)) return finishCmd;

 }
 
 IsSyncResSent = 1;
 // Wait for sync res from C
 if(!syncAckReceived) return finishCmd;
 syncAckReceived = 0;

 while (HAL_CAN_GetTxMailboxesFreeLevel(&hcan) == 0);
 if(!CAN_SendCommand(cmdID2, NULL, NULL)) return finishCmd;

 IsSyncResSent = 0;
 finishCmd = true;
 return finishCmd;
 }
 return finishCmd;
}

Device C:

bool HardSync(uint8_t asyncCmdIdx)
{
 bool finishCmd = false;
 uint32_t startTime = 0;
 PORTAL_COMMANDS cmdID;
 cmdID = SYNC_RES; //0x2BD
 int32_t _timeout = 0;
 
 if(IS_FLAG_SET(portalState, STATE_HARD_SYNC_PENDING) && IS_FLAG_SET(portalState, STATE_HARD_SYNC_WAITING))
 {
 if(!IsSyncStart) return finishCmd;

 IsSyncStart = 0;
 
 if(!CAN_SendCommand(cmdID, NULL, asyncCmdIdx)) 
 return finishCmd;

 uint32_t startTime = HAL_GetTick();
 while (!IsSyncRes)
 {
 if (HAL_GetTick() - startTime > 5000) // 5 seconds
 {
 IsSyncRes = 0;
 return ErrorHandlerSynchronize(asyncCmdIdx, 2);
 }
 }
 
 IsSyncRes = 0;
 
 RESET_FLAG(portalState, STATE_HARD_SYNC_PENDING);
 RESET_FLAG(portalState, STATE_HARD_SYNC_WAITING); 
 
 finishCmd = true;
 return finishCmd;
 }
 return finishCmd;
}

As I said earlier, device B skipped one or two messages from A when sync action takes place between B and C, but it does not happen immediately (for example after 5 successful sync actions then it fails). 

Another thing is take the CAN topology in the line (there are not only 3 CAN devices) is kind of tree/star, which is mistake made from the beginning. However, CAN transmission still works as expected until we have this sync action. The whole CAN line has only 2 terminator resistors (60 ohm is measured). I also tried to set bitrate to 250000 and 125000 bps but it still did not work.

I apologise for the long messages but I hope someone could help me with this.

Thank you in advance.

Best answer by mƎALLEm

@RockCoder wrote:

Hi @mƎALLEm ,

FD and Classic cannot coexist on the same pair of wires unless all nodes are FD-capable?


This paper from www.can-cia.org:  Hybrid CAN and CAN FD networks ,  says:

mALLEm_0-1761321703880.png

 

4 replies

mƎALLEm
ST Technical Moderator
October 24, 2025

Hello @RockCoder and welcome to the community,

More likely it's an implementation issue also depends on the load of your CAN bus.

My comments:

Setting BS2 to 1 is not a good idea. Try to increase BS1 and BS2 to increase them as much as possible and decreasing CAN prescaler. 

I suggest to use CLASSIC frame format from FDCAN sides instead of  FDCAN_FRAME_FD_NO_BRS.

Try to handle the received frames in a ring buffer filled in the Rx call backs and handled in main.

Play with the Rx interrupt priorities.. Increase it.

Check also if a FIFO overrun has occurred: FOVR bit is set in the CAN_RFR register:

The behavior depends on if the FIFO Lock is enabled or disabled:

mALLEm_0-1761309908924.png

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
RockCoderAuthor
Associate
October 24, 2025

Hi @mƎALLEm ,

Thanks for the suggestion. I’d like to sanity-check my bus setup.

  • We have 5+ nodes on the same CAN bus. Only Device B is Classic CAN (bxCAN); the others (including A and C) are FDCAN.

  • Initialization: A/C and the other FD nodes use FDCAN_FRAME_FD_NO_BRS; B is Classic.

  • At runtime:

    • For FD↔FD traffic, A/C set TxHeader.FDFormat = FDCAN_FD_CAN.

    • When A/C talk to B, they switch to TxHeader.FDFormat = FDCAN_CLASSIC_CAN.

Question: On a single physical bus, is this mixed approach actually valid? Or does the presence of a Classic node mean that any FD frame on the wire (even with BRS off) will cause problems—i.e., FD and Classic cannot coexist on the same pair of wires unless all nodes are FD-capable?

 

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
October 24, 2025

@RockCoder wrote:

Hi @mƎALLEm ,

FD and Classic cannot coexist on the same pair of wires unless all nodes are FD-capable?


This paper from www.can-cia.org:  Hybrid CAN and CAN FD networks ,  says:

mALLEm_0-1761321703880.png

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
RockCoderAuthor
Associate
October 28, 2025

The problem was indeed this. I changed the frame format to CLASSIC frame for all my FD CAN controllers and it solved the problem.