Visitor II
January 25, 2021
Question
STEVAL-IME013V1 doesn't connect to Ultrasound Pulser Waveform Demo (STSW-IME011, Error code 2)
- 1 reply
- 1546 views
I have a STEVAL-IME013V1 Evaluation board (STM32 + STHV800) and want to program arbitrary pulse trains with the "Ultrasound Pulser Waveform Demo" (STSW-IME011) with Win10.
- I connect the board via USB.
- I press USR button (LED5 blinks orange) on the board and F5 in the Demo Program
- I get the Error: Connection failed! Unable to retrieve the device type.
- If I select the correct IC (STHV800) then I get Error Code 2
- Reset RST doesn't help
- Changing the baud rate doesn't help
- Adding +5 V/-5 V doesn't help
Pictures of the error, the software version and the board are in the attachment.
Do you have any idea what to do?
Thank you
Best regards
Bjoern
Edit:
I tried it on an old Windows 7 Computer and it worked.
It seems to be a driver problem.