Skip to main content
sabari1
Associate III
September 13, 2023
Question

ST tcp echo client for sending larger data blocks

TCP echo client application running on my STM board and server is run on Linux PC , so here how can I enable the IP fragmentation and reassembly feature in order to transmit/recieve larger chunk of data from my application program to tcp_send/receive functions.

in the example code given from ST i didn't see the fragmentation and reassembly part.(tcp_echo_client for stm32 U585)

or do i need to do manual reassembly in the case of large amount of data(larger than the specified MTU size).

This topic has been closed for replies.