Skip to main content
Visitor
Nov 13, 2026 3:02 AM UTC
Question

ST Edge AI Core 4.1.0 – Smart App Control blocks opt_merge_zero_pad.pyd on Windows 11

Subject: ST Edge AI Core 4.1.0 – Code Integrity blocks unsigned Python modules on Windows 11

Hello ST Support Team,

I am using ST Edge AI Core v4.1.0 (build 4.1.0.20732) with the STM32N6570-DK target to analyze a MobileNetV2 INT8 TFLite model.

When running the stedgeai analyze command, the process fails with the following error:

DLL load failed while importing opt_merge_zero_pad: A policy control application has blocked this file.

System information:

  • Windows 11 Pro, build 26200

  • Python 3.13.12

  • ST Edge AI Core 4.1.0 (build 4.1.0.20732)

  • STM32 MCU module v4.1.0

  • STM32N6 target

Additional investigation:

Windows Smart App Control is enabled.

I checked the Windows Code Integrity Operational log and found Event ID 3077 entries confirming that Windows blocks the following ST Edge AI Core modules:

  1. frontend\concatenate_outputs.cp313-win_amd64.pyd

  2. middleend\opt_merge_zero_pad.cp313-win_amd64.pyd

  3. irs\base\memory_assets.cp313-win_amd64.pyd

The log reports that these files do not meet the Enterprise signing level requirements or violate the active code integrity policy.

I also checked the digital signatures of all .pyd files in the installation directory. All 438 files returned NotSigned using PowerShell's Get-AuthenticodeSignature command.

The SHA256 hash of opt_merge_zero_pad.cp313-win_amd64.pyd is:

FB22EB702ED7C268D9CF74502226A6F8DD1F659E38F9D2C459A39A694A3E5F0B

I have also checked the ST Maintenance Tool, but no updates are available. Restarting Windows did not resolve the issue.

Questions:

  1. Are these .pyd modules expected to be unsigned in ST Edge AI Core 4.1.0?

  2. Is this a known compatibility issue with Windows 11 Smart App Control or Code Integrity policies?

  3. Is there an officially signed replacement, patch, or updated version available?

  4. Is there a recommended and officially supported workaround that allows ST Edge AI Core to run without disabling Smart App Control?

I would appreciate your guidance, as this issue currently prevents me from analyzing models for the STM32N6 target.

Thank you for your assistance.

Best regards

 

1 reply

SlothGrill
ST Employee
Nov 19, 2026 2:26 PM UTC

Hello ​@Stefanos Nerantzoulis 

Thanks for reaching us and pointing out this important information.

  1. Yes: there were no issues up to very recently with providing pyd files unsigned (we never had complaints about that, only the .exe entry points were signed.
  2. Yes: The issue has been internally taken into account ~ 1 week ago, we are working on it.
  3. No: We are working on it.
  4. No: if you absolutely need SmartApp Control, we don’t have any fix for now… we are working on it.

We will keep you posted asap.

 

TL;DR: we are aware of the issue. We feel like this may be a critical one and we are working on it. For now, no workaround available.