Skip to main content
MPatt.11
Associate II
Jan 22, 2019 8:20 PM UTC
Question

SPI Slave transmit has extra byte at times

0690X000006DCWkQAO.jpg0690X000006DCWfQAO.jpg0690X000006DCWaQAO.jpgI have two STM32F7 processors set up in SPI Master/Slave configuration. When the slave wants to transmit data to the master, it issues an interrupt and the master reads 4 bytes. The first two are the number of data bytes to read, the second two is a command code. The master waits for a go-ahead interrupt, then reads the rest of the bytes.

At times, I'm seeing the first byte of the 4-byte transfer duplicated in the data transfer - thus shifting the bytes by one, and adding one byte to the transfer. This may make more sense by looking at the captures from the logic analyzer. I am using HAL_SPI_Transmit_IT to the master, and HAL_SPI_Receive_IT on the master side to receive the bytes.

The transfer rate is 14 MHz. Slowing the clock down makes no difference.

Using SPI_NSS_PULSE_DISABLE or SPI_NSS_PULSE_ENABLE does not help

On the Master side, using SPI_NSS_HARD_OUTPUT or generating the NSS signal manually makes no difference.

The only thing that seems to help is enforcing a minimum transfer rate of 2ms. In other words, the slave needs to wait 2ms minimum between transfers.

Slave initialization:

/* SPI Port for communications with Master processor
 **/
void HAL_SPI_MspInit(SPI_HandleTypeDef* hspi)
{
 GPIO_InitTypeDef GPIO_InitStruct;
 if(hspi->Instance==SPI1)
 {
 /* Peripheral clock enable */
 __HAL_RCC_SPI1_CLK_ENABLE();
 
 /**SPI1 GPIO Configuration 
 PA4 ------> SPI1_NSS
 PA5 ------> SPI1_SCK
 PA6 ------> SPI1_MISO
 PA7 ------> SPI1_MOSI 
 */
 GPIO_InitStruct.Pin = SPI_CS_IN_Pin|SPI_CLK_IN_Pin|SPI_MISO_Pin|SPI_MOSI_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF5_SPI1;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
 
 /* SPI1 interrupt Init */
 HAL_NVIC_SetPriority(SPI1_IRQn, 1, 0); 
 HAL_NVIC_EnableIRQ(SPI1_IRQn);
 }
}
 
 
 
/* SPI1 init function */
void MX_SPI1_Init(void)
{
 /* SPI1 parameter configuration*/
 SPI_SLAVE_1.Instance = SPI1;
 SPI_SLAVE_1.Init.Mode = SPI_MODE_SLAVE;
 SPI_SLAVE_1.Init.Direction = SPI_DIRECTION_2LINES;
 SPI_SLAVE_1.Init.DataSize = SPI_DATASIZE_8BIT;
 SPI_SLAVE_1.Init.CLKPolarity = SPI_POLARITY_LOW;
 SPI_SLAVE_1.Init.CLKPhase = SPI_PHASE_1EDGE;
 SPI_SLAVE_1.Init.NSS = SPI_NSS_HARD_INPUT;
 SPI_SLAVE_1.Init.FirstBit = SPI_FIRSTBIT_MSB;
 SPI_SLAVE_1.Init.TIMode = SPI_TIMODE_DISABLE;
 SPI_SLAVE_1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
 SPI_SLAVE_1.Init.CRCPolynomial = 7;
 SPI_SLAVE_1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
 SPI_SLAVE_1.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
 if (HAL_SPI_Init(&SPI_SLAVE_1) != HAL_OK)
 {
 _Error_Handler(__FILE__, __LINE__);
 }
}

Has anyone seen similar issues with the SPI Slave transfer?

Mark

This topic has been closed for replies.

11 replies

waclawek.jan
Super User
Jun 3, 2023 7:38 AM UTC

Nice list, @S.Ma​ !

> There are different generations of SPI,

... and we still hold our breath until ST kindly supplies us with the list of IP versions used in various STM32 (sub)families... see @Nikita91​ 's Idea... oh wait, Ideas gone thanks to the ST's neglect and salesforce's incompetence...

> the 4..16 bit one, the 32 bit hidden TX/RX FIFO

Is there a 4..16 bit SPI without the FIFO out there?

JW