Skip to main content
Senior
Nov 11, 2024 8:47 PM UTC
Solved

SPI Interrupt Driven Slave Receive Error

I am using STM32H7B3I-DK running a touchgfx application and acting as SPI Master, and Nucleo-H743ZI as SPI Slave. Both are configured in interrupt mode not using HWNSS. 

The Master is sending 1,2,3,4,5,6,7,8 but the slave is receiving random numbers

I am sending one byte at a time and receiving one byte then adding it to a buffer. I want to avoid HAL overhead as much as possible as the data needs to be close to real time. 

The Master seems to send quickly enough using HAL_SPI_Transmit; however, the slave would only receive every other byte, hence the avoidance of HAL on the Slave side.

The master is properly sending data, as checked by oscilloscope. I have double checked the compatible settings for Master-Slave communication in the .ioc files such as Data Size, First Bit, etc...
Here is my following relevant code for the master:

 

 hspi2.Instance = SPI2;
 hspi2.Init.Mode = SPI_MODE_MASTER;
 hspi2.Init.Direction = SPI_DIRECTION_2LINES;
 hspi2.Init.DataSize = SPI_DATASIZE_8BIT;
 hspi2.Init.CLKPolarity = SPI_POLARITY_LOW;
 hspi2.Init.CLKPhase = SPI_PHASE_2EDGE;
 hspi2.Init.NSS = SPI_NSS_SOFT;
 hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_256;
 hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB;
 hspi2.Init.TIMode = SPI_TIMODE_DISABLE;
 hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
 hspi2.Init.CRCPolynomial = 0x0;
 hspi2.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
 hspi2.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;
 hspi2.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;
 hspi2.Init.TxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
 hspi2.Init.RxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
 hspi2.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;
 hspi2.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;
 hspi2.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;
 hspi2.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_ENABLE;
 hspi2.Init.IOSwap = SPI_IO_SWAP_DISABLE;
 if (HAL_SPI_Init(&hspi2) != HAL_OK)
 {
 Error_Handler();
 }

[...]
 for(;;)
	{
		HAL_GPIO_WritePin(GPIOI, GPIO_PIN_0, GPIO_PIN_RESET); // Pull CS low
		HAL_Delay(5);
		for (int i = 0; i < 8; i++) {
			data[i] = i+1;
		 HAL_SPI_Transmit(&hspi2, &data[i], 1, HAL_MAX_DELAY); // Transmit one byte

		}
		HAL_GPIO_WritePin(GPIOI, GPIO_PIN_0, GPIO_PIN_SET); // Pull CS high
		HAL_Delay(100);
 }

 

 

Here is the relevant Slave code:

 

 hspi1.Instance = SPI1;
 hspi1.Init.Mode = SPI_MODE_SLAVE;
 hspi1.Init.Direction = SPI_DIRECTION_2LINES;
 hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
 hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
 hspi1.Init.CLKPhase = SPI_PHASE_2EDGE;
 hspi1.Init.NSS = SPI_NSS_SOFT;
 hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
 hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
 hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
 hspi1.Init.CRCPolynomial = 0x0;
 hspi1.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;
 hspi1.Init.NSSPolarity = SPI_NSS_POLARITY_LOW;
 hspi1.Init.FifoThreshold = SPI_FIFO_THRESHOLD_01DATA;
 hspi1.Init.TxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
 hspi1.Init.RxCRCInitializationPattern = SPI_CRC_INITIALIZATION_ALL_ZERO_PATTERN;
 hspi1.Init.MasterSSIdleness = SPI_MASTER_SS_IDLENESS_00CYCLE;
 hspi1.Init.MasterInterDataIdleness = SPI_MASTER_INTERDATA_IDLENESS_00CYCLE;
 hspi1.Init.MasterReceiverAutoSusp = SPI_MASTER_RX_AUTOSUSP_DISABLE;
 hspi1.Init.MasterKeepIOState = SPI_MASTER_KEEP_IO_STATE_DISABLE;
 hspi1.Init.IOSwap = SPI_IO_SWAP_DISABLE;
 if (HAL_SPI_Init(&hspi1) != HAL_OK)
 {
 Error_Handler();
 }

[...]

void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) {
 if (GPIO_Pin == GPIO_PIN_14) {
 if (HAL_GPIO_ReadPin(GPIOD, GPIO_PIN_14) == GPIO_PIN_RESET) {
 	__HAL_SPI_ENABLE(&hspi1);
 	__HAL_SPI_DISABLE_IT(&hspi1, (SPI_IT_TXP | SPI_IT_DXP | SPI_IT_EOT | SPI_IT_TXTF | SPI_IT_UDR | SPI_IT_OVR | SPI_IT_CRCERR | SPI_IT_FRE | SPI_IT_MODF | SPI_IT_TSERF | SPI_IT_ERR));
 	__HAL_SPI_ENABLE_IT(&hspi1, SPI_IT_RXP);
 }
 }
}


void spiISR(SPI_HandleTypeDef *hspi){
	if (hspi1.Instance->SR & SPI_FLAG_RXP) {

		rxBuffer[rxIndex] = SPI1->RXDR;
		// Increment index and wrap around if necessary
		rxIndex = (rxIndex + 1) % RX_BUFFER_SIZE;
		__HAL_SPI_CLEAR_EOTFLAG(hspi);
		__HAL_SPI_CLEAR_OVRFLAG(hspi);
		__HAL_SPI_CLEAR_FREFLAG(hspi);
	}
}

 

In stm32h7xx_it.c I do the following in the SPI_IRQHandler to avoid calling the large HAL_SPI_IRQHandler :

 

void SPI1_IRQHandler(void)
{
 /* USER CODE BEGIN SPI1_IRQn 0 */
	spiISR(&hspi1);
	return;
 /* USER CODE END SPI1_IRQn 0 */
 HAL_SPI_IRQHandler(&hspi1);
 /* USER CODE BEGIN SPI1_IRQn 1 */

 /* USER CODE END SPI1_IRQn 1 */
}

 

 

 

This topic has been closed for replies.
EthanMankinsBest answer
Senior
Nov 13, 2024 7:56 PM UTC

The issue was likely because of noise. 

FIX: Twisted all com wires tightly: GND SCK MOSI MISO NSS 

7 replies

Pavel A.
Nov 11, 2024 9:09 PM UTC

Have you seen the examples for slave mode in the STM32H7Cube library package? (under Projects dir.)

Senior
Nov 11, 2024 9:50 PM UTC

@Pavel A. 

I have only seen "SPI_FullDuplex_ComIT" which uses the HAL library calls to transmit and receive. I believe I have taken the necessary parts of the HAL functions, Enable() and flag clearing. However, it seems there may be more that I am missing to implement a very basic and quick version of the HAL functions... 

PGump.1
Senior II
Nov 12, 2024 5:46 AM UTC

Hi,

Your code would indicate that the NSS timing is not right. I don't know what you have been looking at on your oscilloscope...

Kind regards
Pedro

AI = Artificial Intelligence, NI = No Intelligence, RI = Real Intelligence.