Skip to main content
Associate III
Sep 30, 2023 5:25 PM UTC
Question

Simple LCD app desired for STM32H747i-DISCO and CubeIDE

I just need to draw some lines and add letters to the MB1166 board's LCD.

The closest application that I've found is targeted for Eclipse, and it's going to be very involved to get it working.

I'm trying to get CubeIDE's TouchGFX application running, but's way too big and complex for what I need.

Help locating a simple CubeIDE LCD driver/application for the H747i-DISCO boards would be greatly appreciated.

This topic has been closed for replies.

4 replies

ST Technical Moderator
Sep 30, 2023 7:05 PM UTC

Hello @BobWalance,

You can start from LCD_DSI examples within STM32CubeIDE, which are available with STM32CubeH7 package: 

STM32CubeH7/Projects/STM32H747I-DISCO/Examples/LCD_DSI at master · STMicroelectronics/STM32CubeH7 · GitHub

More details about LCD configuration provided in:

  • UM2411 User manual Discovery kit with STM32H747XI MCU

Hope this helpful for you!

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Associate III
Sep 30, 2023 8:07 PM UTC

Yes @Imen.D , this is the "Eclipse" application that I mentioned. However, I cannot get it configured properly:

-- I double-click on the '.project' file and STM32CubeIDE starts up and displays this folder in Project Explorer. However, it is not recognized as a proper project (there is no blue IDE logo to the left of LCD_DSI_CmdMode_SingleBuffer).

I can't compile any of the code as is outlined in the 'readme.txt' file. This is where I run into problems with CubeIDE. I'm not sure if I'm supposed to "import" this, and if so how to do the import.

Can you give any tips as to how to proceed?

Thanks for your help on this.

 

Tesla DeLorean
Guru
Sep 30, 2023 7:48 PM UTC

Simple line and text drawing primitives

STM32Cube_FW_H7_V1.9.1\Drivers\BSP\STM32H747I-DISCO\stm32h747i_discovery_lcd.c

STM32Cube_FW_H7_V1.9.1\Projects\STM32H747I-DISCO\Examples\JPEG\JPEG_DecodingUsingFs_Polling\CM7\Src\main.c

 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Associate III
Sep 30, 2023 8:32 PM UTC

Wow @Tesla DeLorean ! This might be just what I was looking for.

I was able to locate both of those files.

Thanks!