Skip to main content
Graduate
Aug 25, 2024 2:46 AM UTC
Question

sensor in X-CUBE-MEMS1

I am using kit board stm32f411vet6 discovery, it has L3gd20 sensor and LSM303DLHC sensor. I want to ask if i can use x-cube-mem1 for L3gd20 and LSM303DLHC because i didn't find one. If x-cube-mem1 is not used then what other library or support software should i use. 

 
This topic has been closed for replies.

3 replies

MOBEJ
ST Employee
Aug 26, 2024 10:13 AM UTC

Hello @ThienNguyen0301 , 

Both of the L3GD20 and LSM303DLHC sensors are already supported in the BSP  examples within the STM32CubeF4 firmware. Specifically, you can refer to the  BSP example for the STM32F411E-Discovery Board by downloading STM32CubeF4 firmware V1.28.0  ( https://www.st.com/en/embedded-software/stm32cubef4.html) .

Please check the BSP example projects (Projects\STM32F411E-Discovery\Examples\BSP) for implementations involving the L3GD20 and LSM303DLHC sensors. This  example will provide you with the necessary code and configurations to use these sensors effectively.

NB : You can utilize these examples to work with your sensors without needing to use the X-CUBE-MEM1 package.

BR

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Aug 26, 2024 11:47 AM UTC

@MOBEJ wrote:

You can utilize these examples to work with your sensors without needing to use the X-CUBE-MEM1 package.


This is, of course, true - but doesn't answer the question:

 


@ThienNguyen0301 wrote:

I want to ask if i can use x-cube-mem1 for L3gd20 and LSM303DLHC  


I don't see either of those sensors mentioned in either the X-CUBE-MEM1 Poduct Page or the UM1859 User Manual:

https://www.st.com/en/embedded-software/x-cube-mems1.html#overview

https://www.st.com/resource/en/user_manual/um1859-getting-started-with-the-xcubemems1-motion-mems-and-environmental-sensor-software-expansion-for-stm32cube-stmicroelectronics.pdf

 

@MOBEJ so are you saying that X-CUBE-MEM1 does not support these sensors?

@ThienNguyen0301 what is it, exactly, from X-CUBE-MEM1 that you want to use?

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
MOBEJ
ST Employee
Aug 26, 2024 1:24 PM UTC

hello @Andrew Neil  , 

yes  , the X-CUBE-MEM1 supports only this feature as described here (X-CUBE-MEMS1 - Sensor and motion algorithm software expansion for STM32Cube - STMicroelectronics) : 

  • motion sensors: A3G4250D, AIS2DW12, AIS2IH, AIS328DQ, AIS3624DQ, ASM330LHH, ASM330LHHX, H3LIS331DL, IIS2DLPC, IIS2ICLX, IIS2MDC, IIS3DWB, ISM303DAC, ISM330DHCX, ISM330DLC, LIS2DH12, LIS2DTW12, LIS2DU12, LIS2DW12, LIS2MDL, LIS3MDL, LSM303AGR, LSM6DSL, LSM6DSO, LSM6DSO32, LSM6DSO32X, LSM6DSOX, LSM6DSR, LSM6DSRX, LSM6DSV16BX, LSM6DSV16X, LSM6DSO16IS
  • pressure sensors: ILPS22QS, ILPS28QSW, LPS22CH, LPS22DF, LPS22HB, LPS22HH, LPS27HHTW, LPS28DFW, LPS33HW, LPS33K
  • infrared sensor: STHS34PF80
  • temperature and humidity sensors: HTS221, STTS22H, STTS751
  • audio sensor: IMP34DT05

BR

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.