Skip to main content
Pilous Droip
Senior
May 21, 2020
Question

Send value in UDP packet

  • May 21, 2020
  • 1 reply
  • 824 views

Hello,

I have a problem. My program doesn't send value in UDP packet and program crash. I try everything, But I didn't find anything.

Some variables and constants

typedef struct UDPsender {
	struct netconn *udp_sender_server;
	struct netbuf *udp_send_buf;
} UDPsender;
 
QueueHandle_t udp_sender_queue = NULL;
 
ip4_addr_t global_udp_ip_address;
int32_t global_udp_port;
 
volatile UDPsender *local_udp_ctx = NULL;
 
void udp_poll(TickType_t timeout);

Init UDP and task for FreeRTOS

int32_t udp_sender_init(UDPsender *udp_ctx, const char *udp_sender_ip_address, const uint16_t udp_sender_port) {
 
	memset(udp_ctx, 0, sizeof(*udp_ctx));
	udp_ctx->udp_send_buf = netbuf_new();
	local_udp_ctx = udp_ctx;
	udp_sender_queue = xQueueCreate(1, sizeof(uint16_t));
 
	inet_pton(AF_INET, udp_sender_ip_address, &global_udp_ip_address);
	global_udp_port = udp_sender_port;
 
	xTaskCreate(udp_sender_task, "UDP_Sender", 500, NULL, 3, NULL);
 
	return 0;
}

Task

void udp_sender_task(void *pvParameters) {
 
	for (;;) {
		udp_poll(10);
	}
}

Receive integer value from queue

void udp_poll(TickType_t timeout) {
 
	static uint16_t value = 0;
 
	if (xQueuePeek(udp_sender_queue, &value, 0) == pdTRUE) {
		while (xQueueReceive(udp_sender_queue, &value, timeout) == pdTRUE) {
			udp_data_send(&value);
		}
	} 
	vTaskDelay(5);
}

And function for sending value.

int32_t udp_data_send(const uint16_t *azimuth) {
 
	local_udp_ctx->udp_sender_server = netconn_new(NETCONN_UDP);
	if (FALSE == IsPtrValid((void*) local_udp_ctx->udp_sender_server)) {
		return (-1);
	}
 
	if (ERR_OK != netbuf_ref(local_udp_ctx->udp_send_buf, azimuth, sizeof(uint16_t))) {
		netconn_close(local_udp_ctx->udp_sender_server);
		netconn_delete(local_udp_ctx->udp_sender_server);
 
		return (-1);
	}
	
	if (netconn_sendto(local_udp_ctx->udp_sender_server, local_udp_ctx->udp_send_buf, &global_udp_ip_address, global_udp_port) != ERR_OK) {
		netconn_close(local_udp_ctx->udp_sender_server);
		netconn_delete(local_udp_ctx->udp_sender_server);
 
		return (-1);
	}
 
	netconn_delete(local_udp_ctx->udp_sender_server);
 
	return 0;
}

 And function for queue (for sending value)

void Send_uint16_to_udp(uint16_t value) {
		xQueueSend(udp_sender_queue, &value, 0);
}

This topic has been closed for replies.

1 reply

Piranha
Principal III
May 30, 2020

> I try everything

No, you haven't - you are not learning from the past and are still using ST's non-working bloatware, which on H7 is incomparably more broken than on any of the older series.

https://community.st.com/s/question/0D50X0000C6eNNSSQ2/bug-fixes-stm32h7-ethernet

https://community.st.com/s/question/0D50X0000AhNBoWSQW/actually-working-stm32-ethernet-and-lwip-demonstration-firmware

In other words it does not work and will not work in a foreseeable future, because the intellectual capability of HAL/Cube developers is too low to even understand these problems.

Compiling from your older topics...

> Can anyone generate a bin file, with some test program? For example: Ping, some web page,......

> I have STM32F767 - Nucleo kit.

Well, take that Nucleo and check out my demo:

https://community.st.com/s/question/0D50X0000AhNBoWSQW/actually-working-stm32-ethernet-and-lwip-demonstration-firmware