Skip to main content
JJoha.4
Associate
Jul 5, 2021 11:54 AM UTC
Question

Seems that the ext_csd commands , used for SANDISK SDMMC cards larger than 1GB has a bug in HAL 1.02.09.

Files with error

HAL 1.02.09

stm32f7xx_II_sdmmc.c,

stm32f7xx_mmc.c.

My EMMC 8GB - SANDISK - SDINBDG4-8G-XA

Seems that the ext_csd, used for cards larger than 1GB has a bug.

MX_SDMMC1_MMC_Init() is exiting with an error.

Fix: for now im using HAL 1.02.08, but then cant use more than 1GB of the 8GB EMMC module.

This topic has been closed for replies.

3 replies

Walid ZRELLI
Visitor II
Jul 7, 2021 9:16 AM UTC

Hello @Jørgen Johannessen​ ,

Welcome to ST Community :)

The request you have raised will be internally checked and treated accordingly to the priority.

We will give you an update as soon as possible.

Thanks for your contribution.

BeST Regards,

Walid

Walid ZRELLI
Visitor II
Jul 7, 2021 9:17 AM UTC

Internal ticket number : 110218

JJoha.4
JJoha.4Author
Associate
Jul 9, 2021 7:47 AM UTC

Get the error 4 in STM32F7XX_HAL_MMC.C line 2776,

 SDMMC_CmdInitTypeDef sdmmc_cmdinit;

 uint32_t errorstate;

 /* Send CMD9 SEND_CSD */

 sdmmc_cmdinit.Argument     = Argument;

 sdmmc_cmdinit.CmdIndex     = SDMMC_CMD_HS_SEND_EXT_CSD;

 sdmmc_cmdinit.Response     = SDMMC_RESPONSE_SHORT;

 sdmmc_cmdinit.WaitForInterrupt = SDMMC_WAIT_NO;

 sdmmc_cmdinit.CPSM       = SDMMC_CPSM_ENABLE;

 (void)SDMMC_SendCommand(SDMMCx, &sdmmc_cmdinit);

 /* Check for error conditions */

// errorstate = SDMMC_GetCmdResp1(SDMMCx, SDMMC_CMD_HS_SEND_EXT_CSD,SDMMC_CMDTIMEOUT);

errorstate = 4.

Have tried to change SDMMC_CMDTIMEOUT to 10000, 20000 but still gets the error.

Best regards

Jørgen Johannessen