Skip to main content
Associate
Apr 16, 2024 7:42 AM UTC
Solved

sdmmc not working with 4-bit mode but working only with 1-bit mode

MCU = STM32L433RCTx

STM32 CubeIDE version - 6.8.0

I'm working on sd card operation using sdmmc 4-bit mode but it is not working. but when I select 1-bit sdmmc mode so it is working as well.

I want to know how can I resolve this issue. my sd card connector is MSD-4-A and there are all line connected with 47k pullup resister leaving CLK pin.

SDMMC Init -

hsd1.Instance = SDMMC1;
hsd1.Init.ClockEdge = SDMMC_CLOCK_EDGE_RISING;
hsd1.Init.ClockBypass = SDMMC_CLOCK_BYPASS_DISABLE;
hsd1.Init.ClockPowerSave = SDMMC_CLOCK_POWER_SAVE_DISABLE;
hsd1.Init.BusWide = SDMMC_BUS_WIDE_4B;
hsd1.Init.HardwareFlowControl = SDMMC_HARDWARE_FLOW_CONTROL_DISABLE;
hsd1.Init.ClockDiv = 4;

there are lots of post available related this issue but can not clear proper solution. In some post there are talking bug in firmware in latest version. if yes so how can I resolve it.

Thanks in advance.

This topic has been closed for replies.

1 reply

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Apr 16, 2024 8:18 AM UTC