Skip to main content
Associate II
Feb 11, 2026 3:40 AM UTC
Question

SDMMC FATFS

Hi ST Community,

I'm facing an issue with FatFs on SDMMC where f_open() or even f_mount() returns FR_DISK_ERR, even though the SD card is initializing correctly at the HAL level.

Here's a summary of the problem and what I’ve verified so far.

  • HAL_SD_Init() completes successfully
  • Card information is read correctly:
    • CID
    • CSD
    • RCA
    • Capacity (LogBlockNbr, LogBlockSize)
  • SDMMC interface appears operational
  • Raw HAL read/write tests (CID/CSD) work fine
I would be grateful if ST experts or anyone familiar with SDMMC + FatFs integration please help me to resolve this issue :
samuel_l_0-1770781136742.png

 

2 replies

ST Technical Moderator
Feb 11, 2026 11:00 AM UTC

Hello @samuel_l 

Please refer to the example FatFs_uSD_Standalone on STM32CubeH7.

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
Andrei Chichak
Lead
Feb 11, 2026 10:57 PM UTC

I expect that the SDCard/eMMC chip is new and does not have a file system on it yet. I.E. it needs to be formatted.