Skip to main content
SHaue.2
Associate
Feb 17, 2023 6:53 PM UTC
Solved

SBSFU settings vs. application settings

I'm running the SBSFU on a STM32H7 where I can succesful upload a new application and it is starting. The application is running on an external flash.

The question is, can I simply change the clock system settings to the applications need at startup or do the bootloader and app must have the same clock settings? Because the bootloader already sets the clock settings for it's own need. Can I use

the same clock settings as it would run as a standalone app?

The second question is, the application is running azure RTOS which uses the SysTick as a base timer und the normal tick is incremented via TIM6. Is this possible to simply change the Tick sources or do I have to stop the current clock system in

any way?

I appriciate your help

This topic has been closed for replies.
Jocelyn RICARD
Jocelyn RICARDBest answer
ST Employee
Apr 21, 2023 5:38 PM UTC

Hello @stefanHriauenstein​,

I'm sorry for late answer.

There is no need to keep the same clocking between bootloader and application.

You just need to be careful when changing the clock, to first disable the PLL.

About your second question, when SBSFU jumps to application it first disable the systick.

So, you don't have to care about how your RTOS is starting.

Best regards

Jocelyn

1 reply

Jocelyn RICARD
Jocelyn RICARDBest answer
ST Employee
Apr 21, 2023 5:38 PM UTC

Hello @stefanHriauenstein​,

I'm sorry for late answer.

There is no need to keep the same clocking between bootloader and application.

You just need to be careful when changing the clock, to first disable the PLL.

About your second question, when SBSFU jumps to application it first disable the systick.

So, you don't have to care about how your RTOS is starting.

Best regards

Jocelyn