Skip to main content
Associate
April 1, 2026
Question

RTOS debugging with CubeIDE

Hi everyone

I've got a few questions about the views that show FreeRTOS Semaphores and Queues:

1.  My application creates a lot of Mutex and Queues, and only the first 63 (or 64 -- I may have lost count) of each type are visible.  Is this a feature or a bug?  And if I want to see the remainder... any thoughts on how to go about that?

2.  Here's a screenshot of the Semaphore view:

SemaphoreList.PNG

2A:  MutexSPI2 is created by CubeMX as a dynamically allocated Mutex using the CMSIS OS wrapper.

2B:  PS-Global Lock is created with 

mutex_init(&lock,"PS-Global Lock");

where

int mutex_init(mutex_t *_m, const char* mutex_name) {
	SemaphoreHandle_t *m = (SemaphoreHandle_t *) _m;
	*m = xSemaphoreCreateMutex();
	vQueueAddToRegistry((QueueHandle_t) m,mutex_name);
	return 0;
}

I'm guessing that since the 'mutex' is being defined as a Semaphore is why it's not showing up on the list as a MUTEX, but I don't understand why the "Size" and "Free" values are.

2C: The remainder of the Semaphores are created by

	ps_queue_t *q = calloc(1, sizeof(ps_queue_t));
	mutex_init(&q->mux, mutex_name);
	semaphore_init(&q->not_empty, 0, sem_name);

 where

int semaphore_init(semaphore_t *_s, unsigned int value, const char* sem_name) {
	SemaphoreHandle_t *s = (SemaphoreHandle_t *) _s;
	*s = xSemaphoreCreateCounting(INT32_MAX, value);
	vQueueAddToRegistry((QueueHandle_t) s,sem_name);
	return 0;
}

I don't understand why the Free and # Blocked Tasks values are so large (other than they look like

pointers to code addresses).

The code does work (I'm using the pubsub-c library from here

https://github.com/jaracil/pubsub-c and modified it so each mutex / semaphore gets assigned

a name so I could tell them apart.

I'm trying to understand what the values mean and if they're important for what I'm using.

Yes, I should probably spend some time reading through the library but was hoping someone could

tell me if it's a feature or a bug...

 

I suppose the biggest question is how this view gets the info it's looking for, and if I'm

mis-interpreting the lists because it's a mutex being viewed as a semaphore, or vice versa.

 

Hope this makes sense to someone other than me, and thank you for your time

 

 

 

1 reply

ST Employee
April 2, 2026

Hello @franticspider787 ,

Thank you for raising these points. 

  1. Why only ~63–64 mutexes/queues are shown?

That’s a limit of STM32CubeIDE’s FreeRTOS awareness plugin, not FreeRTOS itself. The plugin only displays the first N kernel objects (around 64) for performance reasons. Objects beyond that still exist and work; they’re just not listed.

To inspect objects beyond that:

- Register them with vQueueAddToRegistry().
- Use the Expressions / Memory views to inspect the handle directly.

There’s no public setting in CubeIDE to increase this limit.

 

  • Why `Type`, `Size`, `Free`, `#Blocked` look wrong?

The issue is how you add objects to the queue registry. vQueueAddToRegistry() needs the handle, NOT the address of the variable. Passing m/s makes the registry point at the wrong memory, so CubeIDE tries to decode random data as a Queue_t, and by consequence you see huge or strange values for Size, Free, and Blocked tasks.

Correct code should be:

vQueueAddToRegistry((QueueHandle_t)*m, mutex_name);
vQueueAddToRegistry((QueueHandle_t)*s, sem_name);

 

  • Are those values important?

They’re debug info only:

- For a mutex/binary semaphore: Size = 1, Free = 0/1.
- For counting semaphores: Size = max count, Free = current count.
- # Blocked tasks helps diagnose contention.

They don’t affect runtime behavior; wrong values just mean the debugger looked at the wrong memory because of the registry bug, not that your synchronization is broken.

Kind regards, 

DHIF Khaled

"Please mark my answer as best by clicking on the “Accept as solution"" button if it fully answered your question. This will help other users find this solution faster.​"