Skip to main content
Visitor II
Dec 8, 2025 12:02 PM UTC
Question

RTC issue when time goes from 23:59:59 to 00:00:00

Hello,

when my rtc time goes to 23:59:59 to 00:00:00 then my program while loop is slow 
ex. some led toggle with 500ms toggle time is incress X2 
so what is issue?

3 replies

ST Technical Moderator
Dec 8, 2025 1:06 PM UTC

Hello @parthkumar_patel 

Could you please share your code.

Did you measure the toggle time with oscilloscope ? 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
TDK
Dec 8, 2025 1:51 PM UTC

HAL_Delay doesn’t use RTC. The cause has the be something else in your code. You’ll need to share more to diagnose the issue. Look for an interrupt which may be executing then.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Andrew Neil
Super User
Dec 8, 2025 2:02 PM UTC

Welcome to the forum.

As others have said, you need to provide more information.

Please see: 

How to write your question to maximize your chances to find a solution

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.