Skip to main content
Rzh.1
Visitor II
Aug 10, 2022 1:31 AM UTC
Question

RM0383 Rev 3 seems to have some errors in Chapter 22 USB on-the-go full-speed (OTG_FS)

In P687, right bottom part of Figure 248, it says "GRXFSIZ[31:16]", while P715 says that GRXFSIZ[31:16] is "Reserved, must be kept at reset value.".

Besides, also in Figure 248, it says "GNPTXFSIZ", but there is no such register in this Reference Manual. 

I think "GRXFSIZ[31:16]" should be "GRXFSIZ[15:0]" and "GNPTXFSIZ" should be "HNPTXFSIZ/DIEPTXF0", which make sense in this context.

This topic has been closed for replies.

1 reply

KDJEM.1
ST Technical Moderator
Aug 10, 2022 11:24 AM UTC

Hi @Rzh.1​  and welcome to the Community :),

I confirm this issue:

  • In figures 248 and 249 “GRXFSIZ[31:16]�? should be “GRXFSIZ[15:0]�?.
  • In figure 248 “GNPTXFSIZ�? should be “DIEPTXF0�?.
  • In figure 249 “NPTXFSIZ�? should be “HNPTXFSIZ�?.

Thank you for your contribution.

Internal ticket number: 132955 (This is an internal tracking number and is not accessible or usable by customers).

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.