Skip to main content
This topic has been closed for replies.
Imen Ezzine
Imen EzzineBest answer
ST Employee
October 12, 2020

Hi,

Just to be clear the current version we have today for STM32F7x6.svd has reached up to 1.5, and then it got split into different files for each device like STM32F746G.

I did attach the STM32F746.svd file (derived from STM32F7x6.svd) that contains the fix. So in order to replace the older SVD file, you can simply change the name of STM32F746.svd to the name of SVD file you are working with to avoid possible mismatch.

Let me know if this works for you.

-Imen

8 replies

Imen Ezzine
ST Employee
October 9, 2020

Hi rogers ,

It would help more if you can provide the version of the SVD file where you found the problem.

-Imen

PDR
PDRAuthor
Associate II
October 9, 2020

Hi,

I believe it is version 1.1 of STM32F7x.svd. Do I just have an older version? In addition, for the MACFFR register, it has the PAM field named RAM.

In any case, shouldn't the MACDBGR fields be nonzero sometimes? I never see a change.

Thanks!

Pat

Imen Ezzine
ST Employee
October 12, 2020

Hi rogers ,

I did check for you and indeed today we have much more advanced versions for stm32F7.

There is for example a specefic SVD file for  STM32F746 device.

I just need to make sure that the mistakes you reported have been fixed.

I also believe you would be interested in a more recent copy? If that the case let me know and I can share with you.

-Imen

PDR
PDRAuthor
Associate II
October 12, 2020

Hello Imen,

Yes please, an updated version would be much appreciated.

Pat

Imen Ezzine
Imen EzzineBest answer
ST Employee
October 12, 2020

Hi,

Just to be clear the current version we have today for STM32F7x6.svd has reached up to 1.5, and then it got split into different files for each device like STM32F746G.

I did attach the STM32F746.svd file (derived from STM32F7x6.svd) that contains the fix. So in order to replace the older SVD file, you can simply change the name of STM32F746.svd to the name of SVD file you are working with to avoid possible mismatch.

Let me know if this works for you.

-Imen

PDR
PDRAuthor
Associate II
October 12, 2020

Thanks very much Imen!

Do you happen to ave any insights as to getting nonzero values from the MACDBGR fields, now that the SVD description conforms to the RM description? I see no text about enabling, or other required settings.

Pat

Imen Ezzine
ST Employee
October 13, 2020

You are welcome!

Sorry I can't help further, but I believe maybe it would be better to close this thread and create a new one for you second problem.

-Imen

PDR
PDRAuthor
Associate II
October 13, 2020

OK, will do.