Skip to main content
carlosdelfino
Senior
Feb 11, 2025 4:16 AM UTC
Question

RESTful POST requests with LwIP with Nucleo F429ZI

Hi All,
Dears.

I am studying how to make http requests with Nucleo-F429ZI. I have already had success with the web server example (HTTP Server), but now I need to make requests on another server, where a number of endpoints will be available. The difficulty I am having is that all the examples I found use the GET method, and I need to make some requests with the POST method. Is this possible?

Could you recommend some reading material with examples?

This topic has been closed for replies.

1 reply

grd
ST Employee
Jun 23, 2025 3:37 PM UTC

Hi,

the two following references are not HTTP tutorials, but embedded implementation that may be helpful:

 

X-CUBE-CLD-GEN STM32Cube Expansion Package contains application examples which connect to cloud platforms over REST requests.It is based on FreeRTOS kernel and LwIP TCP/IP stack.

The Groovestreams example uses PUT requests.

The Exosite example uses POST requests.

 

For new developments, a maintained embedded library such as coreHTTP could be considered.