Skip to main content
Associate III
Mar 4, 2024 6:13 AM UTC
Solved

Require Support On ULPL and STM32F407

Hello,

Is there any documentation or source code to use ULPL with USB3343? Even I am not cleared USB3343 chip could be used for external High-Speed USB support to STM32F407. Or suggest me any chip with low complexity, I aim to achieve high-speed data transfer from PC to Memory to stream ADC Data and DAC data.

This topic has been closed for replies.
AScha.3
AScha.3Best answer
Super User
Mar 5, 2024 8:39 AM UTC

Hi,

About your idea, to transfer > 10MB/s on USB interface, i think its almost impossible with F4 cpu.

Maybe better idea, to look for interface chip, thats built for such things, like:

FT232HPQ - FTDI (ftdichip.com)

  • USB to synchronous 245 parallel FIFO mode for transfers up to 40 Mbytes/Sec

 

or similar chip...  EZ-USB FX2  or EZ-USB FX3:

EZ-USB™ FX3 USB 5 Gbps Peripheral Controller - Infineon Technologies

  • Up to 32-bits, 100 MHz, parallel general programmable interface (GPIF II)
  • Full accessible 32-bits, 200 MHz, ARM9 core with up to 512 KB of embedded SRAM
If you feel a post has answered your question, please click on " Best Answer ".

2 replies

AScha.3
AScha.3Best answer
Super User
Mar 5, 2024 8:39 AM UTC

Hi,

About your idea, to transfer > 10MB/s on USB interface, i think its almost impossible with F4 cpu.

Maybe better idea, to look for interface chip, thats built for such things, like:

FT232HPQ - FTDI (ftdichip.com)

  • USB to synchronous 245 parallel FIFO mode for transfers up to 40 Mbytes/Sec

 

or similar chip...  EZ-USB FX2  or EZ-USB FX3:

EZ-USB™ FX3 USB 5 Gbps Peripheral Controller - Infineon Technologies

  • Up to 32-bits, 100 MHz, parallel general programmable interface (GPIF II)
  • Full accessible 32-bits, 200 MHz, ARM9 core with up to 512 KB of embedded SRAM
If you feel a post has answered your question, please click on " Best Answer ".
YashJAuthor
Associate III
Mar 5, 2024 10:48 AM UTC

Hi,

I think FT232HPQ IC is a good start for the person who is new to USB protocol. With this chip, STM32H7 could be used?