Skip to main content
Bs.1
Associate III
September 20, 2020
Question

Report descriptor for keyboard

  • September 20, 2020
  • 0 replies
  • 692 views

I want to know how to set report descriptor for keyboard which is going to send 16 byte of data to PC.

I am trying to set default keyboard descriptor as below....

__ALIGN_BEGIN static uint8_t HID_MOUSE_ReportDesc[HID_MOUSE_REPORT_DESC_SIZE] __ALIGN_END =

{

         0x05, 0x01,          // USAGE_PAGE (Generic Desktop)

 0x09, 0x06,          // USAGE (Keyboard)

 0xa1, 0x01,          // COLLECTION (Application)

 0x75, 0x01,          //  REPORT_SIZE (1)

 0x95, 0x08,          //  REPORT_COUNT (8)

 0x05, 0x07,          //  USAGE_PAGE (Keyboard)(Key Codes)

 0x19, 0xe0,          //  USAGE_MINIMUM (Keyboard LeftControl)(224)

 0x29, 0xe7,          //  USAGE_MAXIMUM (Keyboard Right GUI)(231)

 0x15, 0x00,          //  LOGICAL_MINIMUM (0)

 0x25, 0x01,          //  LOGICAL_MAXIMUM (1)

 0x81, 0x02,          //  INPUT (Data,Var,Abs) ; Modifier byte

 0x95, 0x01,          //  REPORT_COUNT (1)

 0x75, 0x08,          //  REPORT_SIZE (8)

 0x81, 0x03,          //  INPUT (Cnst,Var,Abs) ; Reserved byte

 0x95, 0x05,          //  REPORT_COUNT (5)

 0x75, 0x01,          //  REPORT_SIZE (1)

 0x05, 0x08,          //  USAGE_PAGE (LEDs)

 0x19, 0x01,          //  USAGE_MINIMUM (Num Lock)

 0x29, 0x05,          //  USAGE_MAXIMUM (Kana)

 0x91, 0x02,          //  OUTPUT (Data,Var,Abs) ; LED report

 0x95, 0x01,          //  REPORT_COUNT (1)

 0x75, 0x03,          //  REPORT_SIZE (3)

 0x91, 0x03,          //  OUTPUT (Cnst,Var,Abs) ; LED report padding

 0x95, 0x06,          //  REPORT_COUNT (6)

 0x75, 0x08,          //  REPORT_SIZE (8)

 0x15, 0x00,          //  LOGICAL_MINIMUM (0)

 0x25, 0x65,          //  LOGICAL_MAXIMUM (101)

 0x05, 0x07,          //  USAGE_PAGE (Keyboard)(Key Codes)

 0x19, 0x00,          //  USAGE_MINIMUM (Reserved (no event indicated))(0)

 0x29, 0x65,          //  USAGE_MAXIMUM (Keyboard Application)(101)

 0x81, 0x00,          //  INPUT (Data,Ary,Abs)

 0xc0              // END_COLLECTION

};

but using this i can only able to send 6 byte output data to PC instead i want to send 16 bytes.......

Any help regarding this will be highly appreciated........

Thanks in advance.....

This topic has been closed for replies.