Skip to main content
Associate II
Jan 13, 2026 2:19 PM UTC
Solved

Receiving ADF1 data via GPDMA

Hello,

I am trying to get the audio data from ADF1. Therefore I use the GPDMA as shown in this example: https://github.com/STMicroelectronics/STM32CubeU5/tree/main/Projects/STM32U575I-EV/Examples/MDF/ADF_AudioRecorder. I am developing on a B-U585I-IOT02A.

My problem is, that I seem to receive only 0x7FFF. I am not sure I do not receive valid or realistic values. Unlike in the example I want to put the received data in a TX_Queue later and handle them in another task.

Please find my code attached below. I would be very grateful for hints and suggestions.

Thank You!

K.S.

 

MDF_HandleTypeDef AdfHandle0;
MDF_FilterConfigTypeDef AdfFilterConfig0;

DMA_HandleTypeDef handle_GPDMA1_Channel10;

MDF_DmaConfigTypeDef DMAConfig;
int16_t RecBuff[REC_BUFF_SIZE * 2U];
volatile uint32_t DmaRecHalfBuffCplt = 0;
volatile uint32_t DmaRecBuffCplt = 0;

extern DMA_QListTypeDef ADFQueue;

void SystemClock_Config(void);
static void SystemPower_Config(void);
static void MX_GPIO_Init(void);
static void MX_GPDMA1_Init(void);
static void MX_ADF1_Init(void);
static void MX_ICACHE_Init(void);
static void MDF_DMAConfig();


/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* Configure the System Power */
 SystemPower_Config();

 /* Configure the system clock */
 SystemClock_Config();

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_GPDMA1_Init();
 MX_ADF1_Init();
 MX_ICACHE_Init();
 MX_ADFQueue_Config();

 HAL_DMAEx_List_LinkQ(&handle_GPDMA1_Channel10, &ADFQueue);

 MDF_DMAConfig();
 memset(RecBuff, 0x00, sizeof(RecBuff));

 if (HAL_MDF_AcqStart_DMA(&AdfHandle0, &AdfFilterConfig0, &DMAConfig) != HAL_OK)
 {
	 Error_Handler();
 }

 while (1)
 {
	 if (DmaRecHalfBuffCplt == 1)
	 {
		 int16_t a = RecBuff[0];		// RecBuff full of 0x7FFF
		 /**
		 * Here I want to push data from first half of RecBuff into TX_Queue
		 */
		 DmaRecHalfBuffCplt = 0;
	 }

	 if (DmaRecBuffCplt == 1)
	 {
		 int16_t a = RecBuff[128];		// RecBuff full of 0x7FFF
		 /**
		 * Here I want to push second half of RecBuff into TX_Queue
		 */
		 DmaRecBuffCplt = 0;
	 }
 }
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI|RCC_OSCILLATORTYPE_MSIK;
 RCC_OscInitStruct.MSIState = RCC_MSI_ON;
 RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_0;
 RCC_OscInitStruct.MSIKClockRange = RCC_MSIKRANGE_4;
 RCC_OscInitStruct.MSIKState = RCC_MSIK_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI;
 RCC_OscInitStruct.PLL.PLLMBOOST = RCC_PLLMBOOST_DIV4;
 RCC_OscInitStruct.PLL.PLLM = 3;
 RCC_OscInitStruct.PLL.PLLN = 10;
 RCC_OscInitStruct.PLL.PLLP = 32;
 RCC_OscInitStruct.PLL.PLLQ = 2;
 RCC_OscInitStruct.PLL.PLLR = 1;
 RCC_OscInitStruct.PLL.PLLRGE = RCC_PLLVCIRANGE_1;
 RCC_OscInitStruct.PLL.PLLFRACN = 0;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
 |RCC_CLOCKTYPE_PCLK3;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB3CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_4) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief ADF1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_ADF1_Init(void)
{
 /**
 AdfHandle0 structure initialization and HAL_MDF_Init function call
 */
 AdfHandle0.Instance = ADF1_Filter0;
 AdfHandle0.Init.CommonParam.ProcClockDivider = 1;
 AdfHandle0.Init.CommonParam.OutputClock.Activation = ENABLE;
 AdfHandle0.Init.CommonParam.OutputClock.Pins = MDF_OUTPUT_CLOCK_0;
 AdfHandle0.Init.CommonParam.OutputClock.Divider = 4;
 AdfHandle0.Init.CommonParam.OutputClock.Trigger.Activation = DISABLE;
 AdfHandle0.Init.SerialInterface.Activation = ENABLE;
 AdfHandle0.Init.SerialInterface.Mode = MDF_SITF_NORMAL_SPI_MODE;
 AdfHandle0.Init.SerialInterface.ClockSource = MDF_SITF_CCK0_SOURCE;
 AdfHandle0.Init.SerialInterface.Threshold = 31;
 AdfHandle0.Init.FilterBistream = MDF_BITSTREAM0_FALLING;
 if (HAL_MDF_Init(&AdfHandle0) != HAL_OK)
 {
 Error_Handler();
 }

 AdfFilterConfig0.DataSource = MDF_DATA_SOURCE_BSMX;
 AdfFilterConfig0.Delay = 0;
 AdfFilterConfig0.CicMode = MDF_ONE_FILTER_SINC4;
 AdfFilterConfig0.DecimationRatio = 64;
 AdfFilterConfig0.Gain = 0;
 AdfFilterConfig0.ReshapeFilter.Activation = DISABLE;
 AdfFilterConfig0.HighPassFilter.Activation = DISABLE;
 AdfFilterConfig0.SoundActivity.Activation = DISABLE;
 AdfFilterConfig0.AcquisitionMode = MDF_MODE_ASYNC_CONT;
 AdfFilterConfig0.FifoThreshold = MDF_FIFO_THRESHOLD_NOT_EMPTY;
 AdfFilterConfig0.DiscardSamples = 0;
}

/**
 * @brief GPDMA1 Initialization Function
 * @PAram None
 * @retval None
 */
static void MX_GPDMA1_Init(void)
{
 /* Peripheral clock enable */
 __HAL_RCC_GPDMA1_CLK_ENABLE();

 /* GPDMA1 interrupt Init */
 HAL_NVIC_SetPriority(GPDMA1_Channel10_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(GPDMA1_Channel10_IRQn);

 handle_GPDMA1_Channel10.Instance = GPDMA1_Channel10;
 handle_GPDMA1_Channel10.InitLinkedList.Priority = DMA_LOW_PRIORITY_HIGH_WEIGHT;
 handle_GPDMA1_Channel10.InitLinkedList.LinkStepMode = DMA_LSM_FULL_EXECUTION;
 handle_GPDMA1_Channel10.InitLinkedList.LinkAllocatedPort = DMA_LINK_ALLOCATED_PORT0;
 handle_GPDMA1_Channel10.InitLinkedList.TransferEventMode = DMA_TCEM_LAST_LL_ITEM_TRANSFER;
 handle_GPDMA1_Channel10.InitLinkedList.LinkedListMode = DMA_LINKEDLIST_CIRCULAR;
 if (HAL_DMAEx_List_Init(&handle_GPDMA1_Channel10) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel10, DMA_CHANNEL_NPRIV) != HAL_OK)
 {
 Error_Handler();
 }
 __HAL_LINKDMA(&AdfHandle0, hdma, handle_GPDMA1_Channel10);
}

static void MDF_DMAConfig()
{
	DMAConfig.Address		=		(uint32_t)&RecBuff[0];
	DMAConfig.DataLength	=		(REC_BUFF_SIZE * 4U);
	DMAConfig.MsbOnly		= 		ENABLE;
}

void HAL_MDF_AcqHalfCpltCallback(MDF_HandleTypeDef* hmdf)
{
	DmaRecHalfBuffCplt = 1;
}

void HAL_MDF_AcqCpltCallback(MDF_HandleTypeDef* hmdf)
{
	DmaRecBuffCplt = 1;
}

HAL_StatusTypeDef MX_ADFQueue_Config(void)
{
 HAL_StatusTypeDef ret = HAL_OK;
 /* DMA node configuration declaration */
 DMA_NodeConfTypeDef pNodeConfig;

 /* Set node configuration ################################################*/
 pNodeConfig.NodeType = DMA_GPDMA_LINEAR_NODE;
 pNodeConfig.Init.Request = GPDMA1_REQUEST_ADF1_FLT0;
 pNodeConfig.Init.BlkHWRequest = DMA_BREQ_SINGLE_BURST;
 pNodeConfig.Init.Direction = DMA_PERIPH_TO_MEMORY;
 pNodeConfig.Init.SrcInc = DMA_SINC_FIXED;
 pNodeConfig.Init.DestInc = DMA_DINC_INCREMENTED;
 pNodeConfig.Init.SrcDataWidth = DMA_SRC_DATAWIDTH_HALFWORD;
 pNodeConfig.Init.DestDataWidth = DMA_DEST_DATAWIDTH_HALFWORD;
 pNodeConfig.Init.SrcBurstLength = 1;
 pNodeConfig.Init.DestBurstLength = 1;
 pNodeConfig.Init.TransferAllocatedPort = DMA_SRC_ALLOCATED_PORT0|DMA_DEST_ALLOCATED_PORT0;
 pNodeConfig.Init.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER;
 pNodeConfig.TriggerConfig.TriggerPolarity = DMA_TRIG_POLARITY_MASKED;
 pNodeConfig.DataHandlingConfig.DataExchange = DMA_EXCHANGE_NONE;
 pNodeConfig.DataHandlingConfig.DataAlignment = DMA_DATA_RIGHTALIGN_ZEROPADDED;
 pNodeConfig.SrcAddress = 0;
 pNodeConfig.DstAddress = 0;
 pNodeConfig.DataSize = 0;

 /* Build NodeADFRx Node */
 ret |= HAL_DMAEx_List_BuildNode(&pNodeConfig, &NodeADFRx);

 /* Insert NodeADFRx to Queue */
 ret |= HAL_DMAEx_List_InsertNode_Tail(&ADFQueue, &NodeADFRx);

 ret |= HAL_DMAEx_List_SetCircularMode(&ADFQueue);

 return ret;
}
KoCTBest answer
Associate II
Jan 16, 2026 11:39 AM UTC

The code is nearly correct. My problem was a wrong GPIO config. After finding this mistake I could setup a running programm.

However it was really hard to find enaugh and significant information how to setup the GPDMA for such a simple case.

 

1 reply

KoCTAuthorBest answer
Associate II
Jan 16, 2026 11:39 AM UTC

The code is nearly correct. My problem was a wrong GPIO config. After finding this mistake I could setup a running programm.

However it was really hard to find enaugh and significant information how to setup the GPDMA for such a simple case.