Skip to main content
VCasa.1
Associate II
Jul 19, 2020 7:12 PM UTC
Question

Reading .WAV with FATFS and sending it to I2S with DMA

Hello,

I want to implement a wav player from an SD/USB, the problem is with the reading of the data, I have the SD mounted, the wav file opened and when it starts reading-sending it through DMA, it does not work correctly, I have tested a basic sinewave, filling an array with the sine data and sending it with HAL_I2S_Transmit_DMA(), and it works, but when I want a constant buffer reading and sending, what I get is that the audio signal takes a sample, repeats the same sample a few times, and then reads the new sample, it does not have a constant flow of reading-sending.

Here I attach you my main and my waveplayer implementation.

Thank you so much

MAIN.C

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * <h2><center>&copy; Copyright (c) 2020 STMicroelectronics.
 * All rights reserved.</center></h2>
 *
 * This software component is licensed by ST under BSD 3-Clause license,
 * the "License"; You may not use this file except in compliance with the
 * License. You may obtain a copy of the License at:
 * opensource.org/licenses/BSD-3-Clause
 *
 ******************************************************************************
 */
/* USER CODE END Header */
 
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "dma.h"
#include "fatfs.h"
#include "i2c.h"
#include "i2s.h"
#include "sdio.h"
#include "spi.h"
#include "tim.h"
#include "usart.h"
#include "usb_host.h"
#include "gpio.h"
 
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "wav_player.h"
/* USER CODE END Includes */
 
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
 
/* USER CODE END PTD */
 
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define WAV_FILE1 "audio/test.wav"
 
/* USER CODE END PD */
 
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
 
/* USER CODE END PM */
 
/* Private variables ---------------------------------------------------------*/
 
/* USER CODE BEGIN PV */
/*PCM5102_Config PCM5102_1 = {
		.Data_Bits = 16,					// 16, 20, 24, 32
		.FS = FS_441kHz,					// fs
		.LRCK_Frequency = FS_441kHz, 		// fs
		.BCK_Frequency = 32 * FS_441kHz, 	// 32, 48, 64 * fs
};*/
 
 
float mySinVal;
float sample_dt;
uint16_t sample_N;
uint16_t i_t;
 
uint32_t myDacVal;
 
int16_t dataI2S[100];
 
#define PI 3.14159f
 
//Sample rate and Output freq
#define F_SAMPLE		44100.0f
#define F_OUT				80.0f
 
/* USER CODE END PV */
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
void MX_USB_HOST_Process(void);
 
/* USER CODE BEGIN PFP */
 
/* USER CODE END PFP */
 
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
 
/* USER CODE END 0 */
 
/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{
 /* USER CODE BEGIN 1 */
 sample_dt = F_OUT/F_SAMPLE;
 sample_N = F_SAMPLE/F_OUT;
 /* USER CODE END 1 */
 
 /* MCU Configuration--------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_I2C1_Init();
 MX_I2S2_Init();
 MX_SDIO_SD_Init();
 MX_USART1_UART_Init();
 MX_FATFS_Init();
 MX_USB_HOST_Init();
 MX_TIM2_Init();
 MX_TIM3_Init();
 MX_SPI3_Init();
 /* USER CODE BEGIN 2 */
 //TurnOFF the USER LEDs
 HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, RESET);
 HAL_GPIO_WritePin(GPIOA, GPIO_PIN_7, RESET);
 FRESULT res;
 
 if(res = f_mount(&SDFatFS, SDPath, 1) == FR_OK){						//If SD card is correctly mounted
	 HAL_UART_Transmit_IT(&huart1, "SD montada correctamente\n\r", strlen("SD montada correctamente\n\r"));//TX Function
	 //HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, SET);					//Turn ON the LED_1
	 if(wavPlayer_fileSelect("test.wav") == 0){					//If the wav file wasn't correstly opened
		 //HAL_GPIO_WritePin(GPIOA, GPIO_PIN_7, SET);				//Turn ON the LED_2
		 HAL_UART_Transmit_IT(&huart1, "Error al abrir el WAV\n\r", strlen("Error al abrir el WAV\n\r"));//TX Function
	 }
	 else
	 {
		 HAL_UART_Transmit_IT(&huart1, "WAV abierto\n\r", strlen("WAV abierto\n\r"));//TX Function
		 wavPlayer_play();
		 HAL_UART_Transmit_IT(&huart1, "WAV PLAY\n\r", strlen("WAV PLAY\n\r"));//TX Function
		 isPlaying = true;
	 }
 }
 else
 {
	 HAL_UART_Transmit_IT(&huart1, "Error al montar la SD\n\r", strlen("Error al montar la SD\n\r"));//TX Function
	 //HAL_GPIO_WritePin(GPIOA, GPIO_PIN_7, SET);					//Turn ON the LED_2
 }
 
 
 /*
 //Build Sine wave
 	for(uint16_t i=0; i<sample_N; i++)
 	{
 		mySinVal = sinf(i*2*PI*sample_dt);
 		dataI2S[i*2] = (mySinVal )*8000; //Right data (0 2 4 6 8 10 12)
 		dataI2S[i*2 + 1] =(mySinVal )*8000; //Left data (1 3 5 7 9 11 13)
 	}
 
 	HAL_I2S_Transmit_DMA(&hi2s2, (uint16_t *)dataI2S, sample_N*2);
 */
 
 
 
 /* USER CODE END 2 */
 
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */
 MX_USB_HOST_Process();
 
 if(!wavPlayer_isFinished() && isPlaying){
 	 wavPlayer_process();
 }
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}
 
/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
 
 /** Configure the main internal regulator output voltage 
 */
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
 /** Initializes the CPU, AHB and APB busses clocks 
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 4;
 RCC_OscInitStruct.PLL.PLLN = 168;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = 7;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 /** Initializes the CPU, AHB and APB busses clocks 
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
 {
 Error_Handler();
 }
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_I2S;
 PeriphClkInitStruct.PLLI2S.PLLI2SN = 50;
 PeriphClkInitStruct.PLLI2S.PLLI2SR = 2;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
}
 
/* USER CODE BEGIN 4 */
 
/* USER CODE END 4 */
 
/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 
 /* USER CODE END Error_Handler_Debug */
}
 
#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @param file: pointer to the source file name
 * @param line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{ 
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 tex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */
 
/************************ (C) COPYRIGHT STMicroelectronics *****END OF FILE****/

This topic has been closed for replies.

3 replies

VCasa.1
VCasa.1Author
Associate II
Jul 19, 2020 7:12 PM UTC

WAV_PLAYER.C

/*
 * wav_player.c
 *
 * Created on: 17 Apr 2020
 * Author: Mohamed Yaqoob
 */
 
#include "wav_player.h"
#include "fatfs.h"
#include "i2s.h"
 
//WAV File System variables
static FIL wavFile;
 
//WAV Audio Buffer
static uint32_t fileLength;
#define AUDIO_BUFFER_SIZE 4096*1
static uint8_t audioBuffer[AUDIO_BUFFER_SIZE];
static __IO uint32_t audioRemainSize = 0;
WAV_HeaderTypeDef wavHeader;
 
//WAV Player
static uint32_t samplingFreq;
static UINT playerReadBytes = 0;			//Bytes already rode from the file
static bool isFinished=0;
bool isPlaying = false;
 
//WAV Player process states
typedef enum
{
 PLAYER_CONTROL_Idle=0,
 PLAYER_CONTROL_HalfBuffer,
 PLAYER_CONTROL_FullBuffer,
 PLAYER_CONTROL_EndOfFile,
}PLAYER_CONTROL_e;
 
static volatile PLAYER_CONTROL_e playerControlSM = PLAYER_CONTROL_Idle;
 
 
static void wavPlayer_reset(void)
{
 audioRemainSize = 0;
 playerReadBytes = 0;
}
 
/**
 * @brief Select WAV file to play
 * @retval returns true when file is found in USB Drive
 */
bool wavPlayer_fileSelect(const char* filePath)
{
 UINT readBytes = 0;
 //Open WAV file
 if(f_open(&wavFile, filePath, FA_READ) != FR_OK)
 {
 return false;
 }
 //Read WAV file Header
 f_read(&wavFile, &wavHeader, sizeof(wavHeader), &readBytes);
 //Get audio data size
 fileLength = wavHeader.FileSize;
 //Play the WAV file with frequency specified in header
 samplingFreq = wavHeader.SampleRate;
 return true;
}
 
/**
 * @brief WAV File Play
 */
void wavPlayer_play(void)
{
 isFinished = false;
 //Read Audio data from USB Disk
 f_lseek(&wavFile, 0);
 f_read (&wavFile, &audioBuffer[0], AUDIO_BUFFER_SIZE, &playerReadBytes);
 audioRemainSize = fileLength - playerReadBytes;
 //Start playing the WAV
 HAL_I2S_Transmit_DMA(&hi2s2, (uint16_t *)&audioBuffer[0], AUDIO_BUFFER_SIZE);
}
 
/**
 * @brief Process WAV
 */
void wavPlayer_process(void)
{
 switch(playerControlSM)
 {
 case PLAYER_CONTROL_Idle:
 break;
 
 case PLAYER_CONTROL_HalfBuffer:
 playerReadBytes = 0;
 playerControlSM = PLAYER_CONTROL_Idle;
 f_read (&wavFile, &audioBuffer[0], AUDIO_BUFFER_SIZE/2, &playerReadBytes);
 if(audioRemainSize > (AUDIO_BUFFER_SIZE / 2))
 {
 audioRemainSize -= playerReadBytes;
 }
 else
 {
 audioRemainSize = 0;
 playerControlSM = PLAYER_CONTROL_EndOfFile;
 }
 break;
 
 case PLAYER_CONTROL_FullBuffer:
 playerReadBytes = 0;
 playerControlSM = PLAYER_CONTROL_Idle;
 f_read (&wavFile, &audioBuffer[AUDIO_BUFFER_SIZE/2], AUDIO_BUFFER_SIZE/2, &playerReadBytes);
 if(audioRemainSize > (AUDIO_BUFFER_SIZE / 2))
 {
 audioRemainSize -= playerReadBytes;
 }
 else
 {
 audioRemainSize = 0;
 playerControlSM = PLAYER_CONTROL_EndOfFile;
 }
 break;
 
 case PLAYER_CONTROL_EndOfFile:
 f_close(&wavFile);
 wavPlayer_reset();
 isFinished = true;
 playerControlSM = PLAYER_CONTROL_Idle;
 break;
 }
}
 
/**
 * @brief WAV stop
 */
void wavPlayer_stop(void)
{
	HAL_I2S_DMAStop(&hi2s2);
 isFinished = true;
}
 
/**
 * @brief WAV pause/resume
 */
void wavPlayer_pause(void)
{
	HAL_I2S_DMAPause(&hi2s2);
}
void wavPlayer_resume(void)
{
	HAL_I2S_DMAResume(&hi2s2);
}
 
/**
 * @brief isEndofFile reached
 */
bool wavPlayer_isFinished(void)
{
 return isFinished;
}
 
/**
 * @brief Half/Full transfer Audio callback for buffer management
 */
void audioI2S_halfTransfer_Callback(void)
{
 playerControlSM = PLAYER_CONTROL_HalfBuffer;
}
void audioI2S_fullTransfer_Callback(void)
{
 playerControlSM = PLAYER_CONTROL_FullBuffer;
 
 HAL_I2S_Transmit_DMA(&hi2s2, (uint16_t*)&audioBuffer[AUDIO_BUFFER_SIZE / 2], AUDIO_BUFFER_SIZE / 2);
// audioI2S_changeBuffer((uint16_t*)&audioBuffer[0], AUDIO_BUFFER_SIZE / 2);
}
 
/**
 * @brief Half/Full transfer Audio callback for buffer management
 */
 
 
void HAL_I2S_TxCpltCallback(I2S_HandleTypeDef *hi2s)
{
 if(hi2s->Instance == SPI2)
 {
 audioI2S_fullTransfer_Callback();
 }
}
 
void HAL_I2S_TxHalfCpltCallback(I2S_HandleTypeDef *hi2s)
{
 if(hi2s->Instance == SPI2)
 {
 audioI2S_halfTransfer_Callback();
 }
}
 
 

XHuan.1
Associate
Aug 11, 2020 6:35 AM UTC

also have the same problem, were you able to resolve the problem? (I'm using DMA and interrupt for I2S callback and the audio is very choppy

EOrle.1
Visitor II
May 26, 2022 1:51 PM UTC

void HAL_I2S_TxCpltCallback(I2S_HandleTypeDef *hi2s) 

{

if(hi2s->Instance == SPI2)

 {

...

while(hi2s2.hdmatx->State != HAL_DMA_STATE_READY);

HAL_I2S_Transmit_DMA(&hi2s2, (uint16_t*)signal_play_buff, nsamples);

...

}

}