Skip to main content
moreto
Associate II
Jul 13, 2023 11:20 PM UTC
Solved

Re: USB HOST cannot parse the last EndPoint

Dear A.Ziru,

Apparently I'm having the same problem as you when trying to receive MIDI data from a USB device (in this case it's a guitar multi-effects pedalboard). How did you solve the problem? Where and how did you defined that MIDI class descriptor?

In my case, the USBH lig gets stuck in this while loop:

while ((ep_ix < pif->bNumEndpoints) && (ptr < cfg_desc->wTotalLength))

I seems that the function inside the while loop:

pdesc = USBH_GetNextDesc((uint8_t *)(void *)pdesc, &ptr);

never increments the pointers to the end values.

I still need to study more the descriptors and the types of intefaces to better understand what is happening.

I would appreciate if you could indicate the path you followed to solve the problem.

Best regards,

Moreto

    This topic has been closed for replies.
    ABOUA
    ABOUABest answer
    ST Employee
    Aug 18, 2023 8:55 AM UTC

    Hello moreto,

    Just to let you know that the fix of parsing midi interface endpoints is already part of latest host library available under github stm32_mw_usb_host/Core/Src/usbh_ctlreq.c at master · STMicroelectronics/stm32_mw_usb_host · GitHub

    Regards,

    6 replies

    waclawek.jan
    Super User
    Jul 14, 2023 9:06 AM UTC

    This post has been separated from this old thread started by @A.Ziru .

    JW

    mohamed.ayed
    ST Employee
    Jul 21, 2023 10:46 AM UTC

    Hi @moreto and welcome to our community, 

    please can you specify which STM32 target and which middleware version are you using, and how to reproduce this issue ?? 

    Regards.

     

     

     

    moreto
    moretoAuthor
    Associate II
    Jul 24, 2023 2:25 PM UTC

    Hello @mohamed.ayed , thanks!

    The target is a STM32F401RE (from a Nucleo F401RE board) with an external circuit that I build back in 2014 (http://moretosprojects.blogspot.com/2014/12/stm32f4-usb-host-and-device.html)

    The the middleware if from the latest firmware version (I think): V1.27.1

    I would like to mention that I have already found the cause of the problem reported in my question. But I still could not make my host communicate with the device.

    I verified two problems in the USB Host library regarding a device with a complex descriptor, as is my case (a NUX MG-30 guitar pedal).

    1) The MIDI interface endpoint (AudioClass subclass 0x03) has 9 bytes. But the USB HOST library only does this check for subclasses 0x01 and 0x02.

    I changed line 470 of the usbh_ctlreq.c file (in function USBH_ParseCfgDesc)  from:

    if ((pif->bInterfaceClass == 0x01U) && (pif->bInterfaceSubClass == 0x02U))

     to:

    if ((pif->bInterfaceClass == 0x01U) && ((pif->bInterfaceSubClass == 0x02U) || (pif->bInterfaceSubClass == 0x03U)))

    2) The second problem has to do with the total number of interfaces on the device. In my case, the descriptor indicates 4 interfaces. But two of them are dual audio interfaces that the device counts as only one. However the USB HOST library does not take this into account, resulting in 6 interfaces in my case (from 0 to 5). The MIDI interface is number 5. Therefore the USBH_FindInterface function returns the number 5 for the MIDI interface, which generated a non-existent interface error (because in the descriptor the maximum number of interfaces is 4).

    I solved this by modifying the USBH_SelectInterface function.
    I changed line 300 from:

    if (interface < phost->device.CfgDesc.bNumInterfaces)

    to:

    if (interface < USBH_MAX_NUM_INTERFACES)

    I don't know if this is the best solution, but it worked.

    With these modifications and with the inclusion of the MIDI Class functions from https://github.com/rogerallen/stm32disc_midisynth1 the USB HOST library enumerated and detected the device correctly.

    The problem now is that even though I periodically call the USBH_MIDI_Receive function (after the application state is APPLICATION_READY), I get nothing from the device. It seems that my device "does not understand" the host request. The state machine is continuously waiting for the device's response.
    I need to dig a little deeper to better understand what is going on. I am not able to find out, through debug, exactly which bytes the host sends to be able to compare with the data packet sent by the PC (which I was able to get using a USB sniffer).

    If anyone can point me in the right direction to check which bytes the host sends to the device, I would appreciate it!

    Best regards!

    Moreto

    moreto
    moretoAuthor
    Associate II
    Jul 25, 2023 1:52 AM UTC

    If necessary, here is the USB descriptor of my device: https://gist.github.com/miguelmoreto/d1ffd3b25cc04b69ac2a0120e4fc3e24

    ABOUA
    ABOUABest answer
    ST Employee
    Aug 18, 2023 8:55 AM UTC

    Hello moreto,

    Just to let you know that the fix of parsing midi interface endpoints is already part of latest host library available under github stm32_mw_usb_host/Core/Src/usbh_ctlreq.c at master · STMicroelectronics/stm32_mw_usb_host · GitHub

    Regards,