Skip to main content
Visitor II
Oct 24, 2023 7:32 AM UTC
Question

RAM test method for X-CUBE-STL

Hi,

I am reviewing the Safety Manual to utilize the Self-Test Library provided by ST, and I have questions about the RAM Test method.
It is mentioned that STL provides RAM Test using the March C-algorithm, and its verified diagnostic coverage can satisfy 'Medium (90%)'.
I want to develop a product targeting SIL3 of IEC 61508, and if the HFT is structured to satisfy 1, there will be no problem in claiming SIL3 even if the DC is 'Medium (90%)'.
According to Table A.6 of IEC 61508-2 that I checked, the maximum diagnostic coverage that can be achieved with the simple march algorithm is confirmed to be 'Low'. I am curious as to how DC was verified as 'Medium (90%)' in STL.

If there is anything I misunderstand, please give me feedback.

This topic has been closed for replies.

2 replies

Billy OWEN
ST Employee
Oct 25, 2023 7:11 PM UTC

Hi @yang90 

 

The forum moderator had marked your post as needing a little more investigation and direct support. An online support case has been created on your behalf, please stand by for just a moment and you will hear from us.

 

Regards,

Billy

awiernie
Associate III
Mar 14, 2025 8:14 AM UTC

In the 61508-2, the "march" test is mentioned, while the STL used the "march-C" test. The later is much better than other march type tests.