Skip to main content
Senior
Jul 30, 2025 3:24 PM UTC
Solved

Question about TouchSensing

Greetings, 
I have a question about the touchsensing module. I am using a stm32u585rit6 mcu in a custom-made board and making a project using azure rtos. I needed to add touchsensing. I watched the app_azure_rtos_config.h and noticed that there is static memory allocation via threadX memory pools (#define TOUCHSENSING_APP_MEM_POOL_SIZE   5000). Then, at the app_azure_rtos.c file there is the following: 

__ALIGN_BEGIN static UCHAR tsc_byte_pool_buffer[TOUCHSENSING_APP_MEM_POOL_SIZE] __ALIGN_END;
static TX_BYTE_POOL tsc_app_byte_pool;

if (tx_byte_pool_create(&tsc_app_byte_pool, "TOUCHSENSING App memory pool", tsc_byte_pool_buffer, TOUCHSENSING_APP_MEM_POOL_SIZE) != TX_SUCCESS)
 {
 /* USER CODE BEGIN TOUCHSENSING_Byte_Pool_Error */

 /* USER CODE END TOUCHSENSING_Byte_Pool_Error */
 }
 else
 {
 /* USER CODE BEGIN TOUCHSENSING_Byte_Pool_Success */

 /* USER CODE END TOUCHSENSING_Byte_Pool_Success */

 memory_ptr = (VOID *)&tsc_app_byte_pool;
 status = MX_TOUCHSENSING_Init(memory_ptr);
 if (status != TSL_STATUS_OK)
 {
 /* USER CODE BEGIN MX_TOUCHSENSING_Init_Error */
 while(1)
 {
 }
 /* USER CODE END MX_TOUCHSENSING_Init_Error */
 }
 /* USER CODE BEGIN MX_TOUCHSENSING_Init */

 /* USER CODE END MX_TOUCHSENSING_Init */
 }

 

What is the purpose of this memory pool? Is there any thread related to touchsensing running?
Thank you! 

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Aug 11, 2025 4:05 PM UTC

Hello @j_filipe ,

The memory pool in the TouchSensing module is used to reserve a specific memory space for the middleware (MW) functions of the TouchSensing module.
TOUCHSENSING_APP_MEM_POOL_SIZE is generated "hardcoded" by CubeMX. When you have ThreadX + TouchSensing MW, it will add this define, with the default value 5000 in the app_azure_rtos_config.h file, and you can change it manually in the code if needed.
The define itself is used to create the tsc_byte_pool_buffer, used for the memory context of the TouchSensing MW functions.
This "buffer" is a memory space reserved for the MW, so it is not really "used" by the MW directly.
I'll suggest having a look at the official documentation regarding that point:
https://github.com/eclipse-threadx/rtos-docs/blob/main/rtos-docs/threadx/chapter3.md#memory-block-pools

The TouchSensing MW entry point is managed by function "MX_TOUCHSENSING_Init()", and is working in this memory pool.

Hope my answer helps you!

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

2 replies

Imen.DBest answer
ST Technical Moderator
Aug 11, 2025 4:05 PM UTC

Hello @j_filipe ,

The memory pool in the TouchSensing module is used to reserve a specific memory space for the middleware (MW) functions of the TouchSensing module.
TOUCHSENSING_APP_MEM_POOL_SIZE is generated "hardcoded" by CubeMX. When you have ThreadX + TouchSensing MW, it will add this define, with the default value 5000 in the app_azure_rtos_config.h file, and you can change it manually in the code if needed.
The define itself is used to create the tsc_byte_pool_buffer, used for the memory context of the TouchSensing MW functions.
This "buffer" is a memory space reserved for the MW, so it is not really "used" by the MW directly.
I'll suggest having a look at the official documentation regarding that point:
https://github.com/eclipse-threadx/rtos-docs/blob/main/rtos-docs/threadx/chapter3.md#memory-block-pools

The TouchSensing MW entry point is managed by function "MX_TOUCHSENSING_Init()", and is working in this memory pool.

Hope my answer helps you!

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
j_filipeAuthor
Senior
Aug 12, 2025 1:41 PM UTC

Thank you for the input!