Skip to main content
MStew.1
Associate III
Feb 24, 2023 7:53 PM UTC
Solved

Question about the Azure RTOS ThreadX Semaphore example

Hello,

in the Semaphore example(https://community.st.com/s/article/how-does-the-threadx-semaphore-work) there is this step:

Open Core\Src \main.c – you can copy and paste the code below, but please notice the" USER CODE BEGIN", to properly place the code snippet:

/* Private user code ---------------------------------------------------------*/
 
/* USER CODE BEGIN 0 */
 
#define USE_UART_PRINT
 
void __io_putchar(char ch) {
 
#ifdef USE_UART_PRINT
 
 // Code to write character 'ch' on the UART
 
 HAL_UART_Transmit(&huart3, (uint8_t *)&ch, 1, 10);
 
#else
 
 ITM_SendChar(ch);
 
#endif
 
}
 
/* USER CODE END 0 */

The question I have is why is this step and piece of code needed? I understand the previous steps and the code that I need to add in the \app_threadx.c file. But this part I am not sure and it is not explained in the guide.

Can anyone please tell why this part is needed?

Thank you

This topic has been closed for replies.
Haithem Rahmani
Haithem RahmaniBest answer
ST Employee
Feb 25, 2023 1:16 PM UTC

Hi,

this is needed to redirect the printf() output to the serial port.

regards

Haithem

3 replies

Haithem Rahmani
Haithem RahmaniBest answer
ST Employee
Feb 25, 2023 1:16 PM UTC

Hi,

this is needed to redirect the printf() output to the serial port.

regards

Haithem

MStew.1
MStew.1Author
Associate III
Feb 26, 2023 1:35 AM UTC

solved

MStew.1
MStew.1Author
Associate III
Feb 25, 2023 1:19 PM UTC

Ah ok thank you!