Skip to main content
Lukasz Przenioslo
Associate III
March 21, 2018
Question

QSPI + FatFS + USB mass storage

  • March 21, 2018
  • 11 replies
  • 4357 views
Posted on March 21, 2018 at 15:12

Hello there,

I am trying to connect 3 sub-systems:

  • qspi flash memory
  • FatFS
  • USB mass storage device

I have successfully written low level drivers for qspi and have connected it with FatFS middleware. I can read and write file and all- this is working.

Now I need to connect the FatFS layer with USB mass storage layer. I am working with the examples found in CubeMx as well as this:

https://community.st.com/thread/44445-using-fatfs-to-access-sd-card-and-usb-mass-storage-device#comments

My problem is that I quite do not understand how the usb mass storage part reaches for files in the FatFs. I thought at the beginning, that the function pointer for USB mass storage lib would be something like: list files, open file, read file, get file time stamp etc... Now I see that there are function pointers for reading and writing some kind of blocks, which have nothing to do with files in my opinion (at least I see no connection yet):

int8_t STORAGE_Init(uint8_t lun);

int8_t STORAGE_GetCapacity(uint8_t lun, uint32_t *block_num, uint16_t *block_size);

int8_t STORAGE_IsReady(uint8_t lun);

int8_t STORAGE_IsWriteProtected(uint8_t lun);

int8_t STORAGE_Read(uint8_t lun, uint8_t *buf, uint32_t blk_addr, uint16_t blk_len);

int8_t STORAGE_Write(uint8_t lun, uint8_t *buf, uint32_t blk_addr, uint16_t blk_len);

int8_t STORAGE_GetMaxLun(void);

USBD_StorageTypeDef USBD_DISK_fops = {

STORAGE_Init,

STORAGE_GetCapacity,

STORAGE_IsReady,

STORAGE_IsWriteProtected,

STORAGE_Read,

STORAGE_Write,

STORAGE_GetMaxLun,

(int8_t *)STORAGE_Inquirydata,

};

How to translate data from files like language that FatFS is speaking to the language that USB mass storage API will understand? How are FatFs sectors related to USB mass storage blocks?

I would appreciate all help.

#qspi #usb-mass-storage #fatfs

Note: this post was migrated and contained many threaded conversations, some content may be missing.
This topic has been closed for replies.

11 replies

Tesla DeLorean
Guru
March 21, 2018
Posted on March 21, 2018 at 16:04

The underlying media is a block storage system. The ability to store an arbitrary block of data, and then recover that same data at some point in the future.

The FAT File System defines the use of those blocks, the content and structure contained within them.

https://en.wikipedia.org/wiki/Design_of_the_FAT_file_system

 

https://en.wikipedia.org/wiki/File_Allocation_Table

 

The DISKIO layer of the FatFS implementation reads and writes the blocks/sectors on the media. The typical sector size dating back to the CPM and DOS days is 512 bytes. At the time it was an optimal mix of data length vs bit error/detection, and headers, gaps, etc.

Other types of file system include NTFS and UDF

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Lukasz Przenioslo
Associate III
March 21, 2018
Posted on March 21, 2018 at 16:23

Hi

Turvey.Clive

‌ thanks for answer,

I do get the block access idea- in my system 512 bytes is also the block size. The part I dont understand is how to connect FAT filesystem on my device with the USB mass storage link. There are no functions like open file, close file, read file or write file. All there is for the user is to write blocks of data and read them, without any division on files.

So my question is, if I am to write a connection code between FatFS and USB mass storage, how can I overcome this? I understand the concept of file system, i dont understand how to deliver it to the USB mass storage part.

For example: Imagine I have already created 3 files and wrote something to them. They reside in my file system. On the FatFs interface part I do not know where exactly they are in the filesystem and how are they distributed in the memory. I access them through f_open, f_read etc. The USB mass storage on the other hand requires block addresses and sizes. How to connect this?

Tesla DeLorean
Guru
March 21, 2018
Posted on March 21, 2018 at 16:42

ST's method is to have a 'wedge' DISKIO implementation for FATFS that vectors the block IO calls to the specific storage layer/drive being used. So you have a structure of function pointers, one goes to SDIO/SDMMC, another to USBSTOR/MSC, QSPI, NOR/NAND, etc.

/**

  * @brief  Gets Disk Status

  * @param  pdrv: Physical drive number (0..)

  * @retval DSTATUS: Operation status

  */

DSTATUS disk_status (

    BYTE pdrv        /* Physical drive number to identify the drive */

)

{

  DSTATUS stat;

  stat = disk.drv[pdrv]->disk_status(disk.lun[pdrv]);

  return stat;

}

/**

  * @brief  Initializes a Drive

  * @param  pdrv: Physical drive number (0..)

  * @retval DSTATUS: Operation status

  */

DSTATUS disk_initialize (

    BYTE pdrv                /* Physical drive nmuber to identify the drive */

)

{

  DSTATUS stat = RES_OK;

  if(disk.is_initialized[pdrv] == 0)

  {

    disk.is_initialized[pdrv] = 1;

    stat = disk.drv[pdrv]->disk_initialize(disk.lun[pdrv]);

  }

  return stat;

}

/**

  * @brief  Reads Sector(s)

  * @param  pdrv: Physical drive number (0..)

  * @param  *buff: Data buffer to store read data

  * @param  sector: Sector address (LBA)

  * @param  count: Number of sectors to read (1..128)

  * @retval DRESULT: Operation result

  */

DRESULT disk_read (

    BYTE pdrv,        /* Physical drive nmuber to identify the drive */

    BYTE *buff,        /* Data buffer to store read data */

    DWORD sector,            /* Sector address in LBA */

    UINT count        /* Number of sectors to read */

)

{

  DRESULT res;

  res = disk.drv[pdrv]->disk_read(disk.lun[pdrv], buff, sector, count);

  return res;

}

The MSC implementation has to provide a number of SCSI/ATAPI-MMC type commands (READ, WRITE, TEST-UNIT-READY, GET CAPACITY, INQUIRY, etc), as your Windows/Linux system sends IO requests to the media, and implements the FAT, NTFS, UDF etc with File System drivers on the host, NOT on the flash stick or external hard drive.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..