Skip to main content
FDanf.1
Visitor II
Oct 10, 2022 7:14 PM UTC
Solved

QSPI Data line always high after HAL initialization on B-L462E-CELL1 devkit

I'm trying to use the QSPI interface in Indirect mode to read, write, and erase to an MT25Q Flash chip that is found on the B-L462E-CELL1 development kit.

Using the HAL QSPI initilization included in the STM32CubeL4 package, I am finding the interface misconfigured. The IO3 data line idles high, while all others idle low.

Additionally, it looks like the QSPI peripheral is using all 4 IO lines for instructions, addresses, and data even though I am specifying 1_LINE in each QSPI command, as evidenced by the number of cycles

Are there any known issues with this HAL package?

0693W00000UnkU0QAJ.png

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Oct 10, 2022 9:15 PM UTC

D3 would normally be HOLD# or RESET#, Micron says this should be pulled high with devices in single or dual mode. On some of their BGA parts RESET# is pulled high via an internal pull up, and can be left unconnected.

The memory device should only care about the state of the lines when it's CS# is asserted. The subset of pins involved depends on the mode the device is in.

Not sure of the code or expectations on the B-L462E-CELL1 board. The BSP normally walks the chip into the desired mode of operation, XIP usage would end that with a Memory Mapping configuration.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

1 reply

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Oct 10, 2022 9:15 PM UTC

D3 would normally be HOLD# or RESET#, Micron says this should be pulled high with devices in single or dual mode. On some of their BGA parts RESET# is pulled high via an internal pull up, and can be left unconnected.

The memory device should only care about the state of the lines when it's CS# is asserted. The subset of pins involved depends on the mode the device is in.

Not sure of the code or expectations on the B-L462E-CELL1 board. The BSP normally walks the chip into the desired mode of operation, XIP usage would end that with a Memory Mapping configuration.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..