Skip to main content
maelli
Associate
Mar 2, 2020 7:03 PM UTC
Question

PWM DMA: Interrupt Callback not working on STM32L452

Sorry if the question sounds stupid, I am new to STM32.

I managed to have a PWM working, timer 1, pos/negative, deadtime, working with DMA from an array with pre-calculated values.

 HAL_TIM_PWM_Start_DMA(&htim1, TIM_CHANNEL_1, sine_val, samples);

 HAL_TIMEx_PWMN_Start(&htim1, TIM_CHANNEL_1);

What does not work for me are the complete and halfcomplete interrupts.

HAL_DMA_IRQHandler gets called in the stm32l4xx_it.c file.

However, in main.c nothing happens:

/* USER CODE BEGIN 4 */

void HAL_DMA_XferHalfCpltCallback(DMA_HandleTypeDef *hdma)

{

GPIOA->ODR ^=GPIO_ODR_OD5; //does not get here

}

/* USER CODE END 4 */

Is there anything I am doing horribly wrong?

Do I need to explicitely enable DMA irqs?

Thanks for any hints

This topic has been closed for replies.