Skip to main content
Associate
Nov 26, 2024 3:29 PM UTC
Question

Programming with USB C and communication via UART

Good morning everyone!

I have a question regarding a USB to UART IC. I’ve seen that the FT231XQ is used in ESP32s to program and communicate via UART. Is it possible to do the same with STM32s?

 

This topic has been closed for replies.

3 replies

Andrew Neil
Super User
Nov 26, 2024 3:50 PM UTC

Yes.

In this case, all the STM32 sees is a UART connection - it neither knows nor cares whether that came via USB, or from a Real RS232 port, or from anything else.

So, as far as the STM32 is concerned, the FT231XQ (or whatever) is irrelevant - it's all just UART comms.

The built-in UART Bootloader is described in Application Note AN3155, USART protocol used in the STM32 bootloader:

https://www.st.com/resource/en/application_note/an3155-usart-protocol-used-in-the-stm32-bootloader-stmicroelectronics.pdf

 

You can also write your own custom bootloader - see, for example Application Note AN4657 STM32 in-application programming (IAP) using the USART:

https://www.st.com/resource/en/application_note/an4657-stm32-inapplication-programming-iap-using-the-usart-stmicroelectronics.pdf

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Zero-96Author
Associate
Nov 26, 2024 6:46 PM UTC

Okay, for Uart it will be possible, but to upload programs to the MCU, will it be possible?

Andrew Neil
Super User
Nov 27, 2024 8:53 AM UTC

@Zero-96 wrote:

Okay, for Uart it will be possible, but to upload programs to the MCU, will it be possible?


I don't understand - I just answered exactly that question!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.