Associate
Jun 11, 2018 6:33 AM UTC
Question
Program doesn't run properly when debugger is not connected in STM32L476RE MCU
- 27 replies
- 8387 views
Posted on June 11, 2018 at 08:33
Hello,
I am using STM32L476RE MCU for one of my application which publishes some data to server using MQTT and my wifi module communicates with MCU with USART2.I am using atollic truestudio to write a code and debug it.I am using ST LINK V2 as my debugger.Now the problem that i am facing is that when i flash a code to MCU and debugger is connected then it runs fine but as soon as i remove debugger and turn off power and again power up the circuit then it doesnt work.I wrote a simple code for GPIO toggling it runs fine without debugger connected.I have attached the code that i have wrote.Same code works absolutely fine with STM32F401RE.Please help as soon as possible.
Regards,
Pradeep Choudhary
#stlink-v2 #stm32l4 #por-issue Note: this post was migrated and contained many threaded conversations, some content may be missing.