Skip to main content
MEhrh.894
Visitor II
November 6, 2019
Question

Problems with DFU bootloader for STM32G431

I want to program my STM32G431-Board with the DFU bootloader.

I’ve already set the configuration to get into the boot-mode with the boot0-Pin. And I explicit configure the read out protection (RDPto level 0.

Also I can connect the device with the USB already in the CubeProgrammer.

My problem is, when I would start programming my code to the target with the CubeProgrammer, there are the following error-message:

Error: RDP level is set to 1 (0xBB), try using Read UnProtect (-rdu) command in order to remove the Read Out Protection.

When I look to the configuration after the error-message, the RDP is on level 0, like I configure before.

This topic has been closed for replies.