Skip to main content
Associate
Apr 30, 2025 1:49 AM UTC
Solved

Problem with IPC on STM32H747I-DISCO

Good morning everyone, I have been trying for two days now to perform a communication between the two cores of STM32H747I-DISCO. Being my first time to try my hand at dual core Processors I decided to start from tutorials:
- https://www.youtube.com/watch?v=MLcULDnF5ic
- https://www.youtube.com/watch?v=miUzjoe3rAo&t=561s (Also the precendent videos

Although I followed these tutorials step by step (without even changing the names to the variables) I could not get it to work at all.

I then also tried with the "PingPong" example directly from STMCubeIDE but with both RTOS and bareMetal versions it didn't work...

The only thing I can think of is that maybe I need to move some jumpers on the board or something....


Thanks in advance to everyone

P.S.
FW H7 Version 1.12.1
STMCubeIDE Version 1.18.0
STMCubeMX Version 6.13.0

Translated with DeepL.com (free version)

This topic has been closed for replies.
KORKAD
KORKADBest answer
ST Technical Moderator
Apr 30, 2025 1:53 PM UTC

Hello @Nikbia,

Please check the OpenAMP applications available in the STM32CubeH7 firmware package. Below is the link to download the package: STM32CubeH7.

Two OpenAMP applications are available for the STM32H747I-DISCO board and run without any hardware configuration (located in Projects\STM32H747I-DISCO\Applications\OpenAMP).

Please refer to the readme.txt file available within each project for technical details.

With Regards,

Anis

 

 

5 replies

KORKAD
KORKADBest answer
ST Technical Moderator
Apr 30, 2025 1:53 PM UTC

Hello @Nikbia,

Please check the OpenAMP applications available in the STM32CubeH7 firmware package. Below is the link to download the package: STM32CubeH7.

Two OpenAMP applications are available for the STM32H747I-DISCO board and run without any hardware configuration (located in Projects\STM32H747I-DISCO\Applications\OpenAMP).

Please refer to the readme.txt file available within each project for technical details.

With Regards,

Anis

 

 

NikbiaAuthor
Associate
May 6, 2025 9:51 PM UTC

After creating a new Workspace and a new project (As you said from the OpenAMP_PingPong example) It worked. 
Now I'm comparing the different tutorial on YT with the content of the example project but unluckly there's no .ioc file for the example...

Still I will try to create a running version using this example as reference and I will let you know.

Associate III
May 2, 2025 1:20 AM UTC

Hi @Nikbia ,

I think this video tutorial is very helpful for understanding how OpenAMP is used with FreeRTOS. I recommend checking it out:
The BEST OpenAMP project implementation on STM32H747 with TouchGFX analogy clock

NikbiaAuthor
Associate
May 6, 2025 9:53 PM UTC

Thanks for the invise. I looked it up but it doesn't do much different from the other videos and i thinks that the implementation with TouchGFX and also the RTC makes it even more confunsing (Due to it's "Special" Clock setup).

Anyways thank you for your help ;) .