Skip to main content
Associate
Feb 22, 2024 4:36 PM UTC
Question

Problem with "HAL_UARTEx_ReceiveToIdle_DMA"

Hi,

I am using the HAL function "HAL_UARTEx_ReceiveToIdle_DMA" as follows:

void HAL_UARTEx_ReceiveToIdle_DMA(UART_HandleTypeDef *huart, uint16_t Size) {

//my actions

HAL_UARTEx_ReceiveToIdle_DMA(peripheral, buffer, COMMAND_MAXIMUM_LENGTH);

__HAL_DMA_DISABLE_IT(peripheral_dma, DMA_IT_HT);

}

It always works fine after I power up the MCU. I was continuously sending UART frames from my computer to the MCU for 2 days and it worked fine. The idle interruption was always detected.

But when I stop sending frames and then start sending them again (by disconnecting and reconnecting the TX wire), the IDLE interruption is no longer detected… until I turn off and power up the MCU again.

 

Why?

 

 

This topic has been closed for replies.

7 replies

TDK
Feb 22, 2024 4:43 PM UTC

Probably a bug in your code. Debug the code, pause, and examine the state of the software state machine in huart. Also look for error flags in the UART registers.

> by disconnecting and reconnecting the TX wire

So the TX line floats? Perhaps triggering a frame error. Do you check for and clear those?

"If you feel a post has answered your question, please click ""Accept as Solution""."
areyzummoAuthor
Associate
Feb 22, 2024 5:36 PM UTC

The UART registers look nice. Indeed, the ‘HAL_UARTEx_ReceiveToIdle_DMA’ returned HAL_OK the last time before disconnecting.

The TX is not floating.

The interrupt just disables itself. This is because if I put this code inside the while(1) loop:

HAL_UARTEx_ReceiveToIdle_DMA(peripheral, buffer, COMMAND_MAXIMUM_LENGTH);

__HAL_DMA_DISABLE_IT(peripheral_dma, DMA_IT_HT);

It works perfectly...

 

Why interruption is disable itself?

TDK
Feb 22, 2024 10:27 PM UTC

> The UART registers look nice.

What does this even mean? "Nice" is not objective. Show them, do they indicate an error, do they indicate a transfer in progress? Show the contents of the huart structure. Same questions.

Likely this mystery could be solved within a few minutes of looking into those structures when the problem happens.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Bob S
Super User
Feb 22, 2024 9:18 PM UTC

> Why interruption is disable itself?

It doesn't.  Some code somewhere is disabling it.  Do you have an error callback function - HAL_UART_ErrorCallback()?  You should.  That will show you if you get errors as mentioned by @TDK

EDIT: The HAL UART code will disable the UART (and interrupts) when it detects an error.  That error callback it the way you detect that this has happened

areyzummoAuthor
Associate
Feb 23, 2024 9:00 AM UTC

When I say that I disconnect the transmission, it means that I am disconnecting the wire. All the frames I see on my logic analyzer and oscilloscope are correct, with no glitches or noise.

However, you are right. When I disconnect, my code enters the function HAL_UART_ErrorCallback() and displays sometimes:

HAL_UART_ERROR_FE 0x00000004U /*!< Frame error */.

and other times:

HAL_UART_ERROR_DMA 0x00000010U /*!< DMA transfer error */

I don’t know what causes that error, because it always happens, even sometimes when I disconnect while no frames are being transmitted.

Okay, thank you. I didn’t know about that ErrorCall function. I was debugging by looking at the Huart structure, but since I always stop inside my code, the error code was always correct.

Thank you very much

 

TDK
Feb 23, 2024 2:39 PM UTC

If a frame error is being flagged, the data is likely not as glitchless and noise-free as you are interpreting. Note that a logic analyzer typically may only interpret based on edges.

"If you feel a post has answered your question, please click ""Accept as Solution""."