Skip to main content
Duddie
Associate II
Aug 16, 2020 3:00 PM UTC
Solved

Problem with HAL_I2S_Transmit_DMA on STM32H750

Hi!

I have tried to use I2S onn STM32H750 and DMA has no success. I can transfer without problem data by standard HAL_I2S_Transmit but HAL_I2S_Transmit_DMA results in Error callback being fired although function itself completes with HAL_OK.

I2S Config

 hi2s2.Instance = SPI2;
 hi2s2.Init.Mode = I2S_MODE_MASTER_TX;
 hi2s2.Init.Standard = I2S_STANDARD_PCM_SHORT;
 hi2s2.Init.DataFormat = I2S_DATAFORMAT_32B;
 hi2s2.Init.MCLKOutput = I2S_MCLKOUTPUT_ENABLE;
 hi2s2.Init.AudioFreq = I2S_AUDIOFREQ_48K;
 hi2s2.Init.CPOL = I2S_CPOL_LOW;
 hi2s2.Init.FirstBit = I2S_FIRSTBIT_MSB;
 hi2s2.Init.WSInversion = I2S_WS_INVERSION_DISABLE;
 hi2s2.Init.Data24BitAlignment = I2S_DATA_24BIT_ALIGNMENT_LEFT;
 hi2s2.Init.MasterKeepIOState = I2S_MASTER_KEEP_IO_STATE_DISABLE;

DMA Config:

 hdma_spi2_tx.Instance = DMA1_Stream5;
 hdma_spi2_tx.Init.Request = DMA_REQUEST_SPI2_TX;
 hdma_spi2_tx.Init.Direction = DMA_MEMORY_TO_PERIPH;
 hdma_spi2_tx.Init.PeriphInc = DMA_PINC_DISABLE;
 hdma_spi2_tx.Init.MemInc = DMA_MINC_ENABLE;
 hdma_spi2_tx.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;
 hdma_spi2_tx.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;
 hdma_spi2_tx.Init.Mode = DMA_CIRCULAR;
 hdma_spi2_tx.Init.Priority = DMA_PRIORITY_HIGH;
 hdma_spi2_tx.Init.FIFOMode = DMA_FIFOMODE_ENABLE;

And when I fire:

res = HAL_I2S_Transmit_DMA(&hi2s2, (uint16_t*)buf, buf_size);

I end up with Callback

void HAL_I2S_ErrorCallback(I2S_HandleTypeDef *hi2s) 

being called.

Other callbacks like HAL_I2S_TxHalfCpltCallback or HAL_I2S_TxCpltCallback never get called.

Is there any extra bit I need to do? Can I run any other diagnostics? I see that DMA interrupt is called and there is TransmitError happening.

This topic has been closed for replies.
Duddie
DuddieBest answer
Associate II
Aug 16, 2020 3:30 PM UTC

Found a problem. For those not familiar with H7 series like me, the DMA operates only from D1/D2 memories and therefore its buffer needs to be allocated there.

1 reply

Duddie
DuddieAuthorBest answer
Associate II
Aug 16, 2020 3:30 PM UTC

Found a problem. For those not familiar with H7 series like me, the DMA operates only from D1/D2 memories and therefore its buffer needs to be allocated there.