Skip to main content
smok.1
Visitor II
Jun 2, 2023 6:42 AM UTC
Question

Problem with FreeRTOS ISR Task Notification

I am using Nucleo F411RE dev borad. When I using the FreeRTOS, I found that the xTaskNotifyFromISR always stuck.

my handler function as below and I can enter it normally.

the program stop at

---------------------------------------------------------------------------
 
/* USER CODE BEGIN 4 */
 
 
 
void button_interrupt_handler(void) {
 
	SEGGER_SYSVIEW_PrintfTarget("button_interrupt_handler\n");
 
	BaseType_t pxHigherPriorityTaskWoken;
 
 
 
	pxHigherPriorityTaskWoken = pdFALSE;
 
 
 
	traceISR_ENTER();
 
	SEGGER_SYSVIEW_PrintfTarget("next_task_handle %X\n",next_task_handle);
 
	SEGGER_SYSVIEW_PrintfTarget("eNoAction %X\n",eNoAction);
 
	SEGGER_SYSVIEW_PrintfTarget("pxHigherPriorityTaskWoken %X\n",pxHigherPriorityTaskWoken);
 
	xTaskNotifyFromISR(next_task_handle, 0, eNoAction, &pxHigherPriorityTaskWoken);
 
	//xTaskNotify(task2_handle, 0, eNoAction);
 
 
 
	/* once the ISR exits, the below macro makes higher priority task which got unblocked to resume on the CPU */
 
	portYIELD_FROM_ISR(pxHigherPriorityTaskWoken);
 
 
 
	traceISR_EXIT();
 
}
 
 
 
 
 
	xTaskNotifyFromISR(next_task_handle, 0, eNoAction, &pxHigherPriorityTaskWoken);
 
 
 
-------------------------------------------------------------------------

I follow the trace and the finialy stop at

------------------------------------------------
 
 configASSERT( xTaskToNotify );
 
 
 
----------------------------------------------------

in the tasks.c file of FreeRTOS

The actual function as below

----------------------------------------------------------
 
#if ( configUSE_TASK_NOTIFICATIONS == 1 )
 
 
 
 BaseType_t xTaskGenericNotifyFromISR( TaskHandle_t xTaskToNotify,
 
 UBaseType_t uxIndexToNotify,
 
 uint32_t ulValue,
 
 eNotifyAction eAction,
 
 uint32_t * pulPreviousNotificationValue,
 
 BaseType_t * pxHigherPriorityTaskWoken )
 
 {
 
 TCB_t * pxTCB;
 
 uint8_t ucOriginalNotifyState;
 
 BaseType_t xReturn = pdPASS;
 
 UBaseType_t uxSavedInterruptStatus;
 
 
 
 configASSERT( xTaskToNotify );
 
 configASSERT( uxIndexToNotify < configTASK_NOTIFICATION_ARRAY_ENTRIES );
 
 
 
 /* RTOS ports that support interrupt nesting have the concept of a
 
 * maximum system call (or maximum API call) interrupt priority.
 
 * Interrupts that are above the maximum system call priority are keep
 
 * permanently enabled, even when the RTOS kernel is in a critical section,
 
 * but cannot make any calls to FreeRTOS API functions. If configASSERT()
 
 * is defined in FreeRTOSConfig.h then
 
 * portASSERT_IF_INTERRUPT_PRIORITY_INVALID() will result in an assertion
 
 * failure if a FreeRTOS API function is called from an interrupt that has
 
 * been assigned a priority above the configured maximum system call
 
 * priority. Only FreeRTOS functions that end in FromISR can be called
 
 * from interrupts that have been assigned a priority at or (logically)
 
 * below the maximum system call interrupt priority. FreeRTOS maintains a
 
 * separate interrupt safe API to ensure interrupt entry is as fast and as
 
 * simple as possible. More information (albeit Cortex-M specific) is
 
 * provided on the following link:
 
 * https://www.FreeRTOS.org/RTOS-Cortex-M3-M4.html */
 
 portASSERT_IF_INTERRUPT_PRIORITY_INVALID();
 
 
 
 pxTCB = xTaskToNotify;
 
 
 
 uxSavedInterruptStatus = portSET_INTERRUPT_MASK_FROM_ISR();
 
 {
 
 if( pulPreviousNotificationValue != NULL )
 
 {
 
 *pulPreviousNotificationValue = pxTCB->ulNotifiedValue[ uxIndexToNotify ];
 
 }
 
 
 
 ucOriginalNotifyState = pxTCB->ucNotifyState[ uxIndexToNotify ];
 
 pxTCB->ucNotifyState[ uxIndexToNotify ] = taskNOTIFICATION_RECEIVED;
 
 
 
 switch( eAction )
 
 {
 
 case eSetBits:
 
 pxTCB->ulNotifiedValue[ uxIndexToNotify ] |= ulValue;
 
 break;
 
 
 
 case eIncrement:
 
 ( pxTCB->ulNotifiedValue[ uxIndexToNotify ] )++;
 
 break;
 
omit................
 
-----------------------------------------------------------

Anyone have similar case?

This topic has been closed for replies.

1 reply

gbm
Super User
Jun 2, 2023 7:51 AM UTC

Read the comment you found in FreeRTOS code and apply it. The interrupt using FreeRTOS sync mechanisms must have priority numerically higher (=logically lower) than FreeRTOS call priority.

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice