Skip to main content
Mohammad Hossein
Associate II
November 30, 2017
Question

Problem with FFT Functions in FreeRTOS

  • November 30, 2017
  • 2 replies
  • 1226 views
Posted on November 30, 2017 at 09:06

Hello,

I'm running freeRTOS on STM32F4. I have no problem with using

cmsis-dsp

functions without freeRTOS.

But when I want to call a function (in which cmsis-dsp functions like arm_cfft_radix4_f3,arm_rfft_f32 ,... are called) from a task(thread):

1.If I pass local arrays (defined in that task) as fft input and output ,output becomes zero!!

2.If I pass global arrays, I have non-zero(correct) output, but using global variables in freeRTOS tasks can cause some problems as we know.

3.If I pass global arrays as fft input and output but send output to another task using queues I receive zero values there!!

I don't know if there is problem with freeRTOS variables that is defined in its heap and cmsis-dsp functions defined out of  freeRTOS heap. 

Here is my code:

// fft function

void waveformFFT(float32_t *input,float32_t *output,uint16_t fftSize)

{

arm_cfft_radix4_instance_f32 fftStruct;

arm_cfft_radix4_init_f32(&fftStruct,fftSize,0,1);

arm_cfft_radix4_f32(&fftStruct,input);

arm_cmplx_mag_f32(input, output, fftSize);

}

 // waveformProcess task

void waveformProccess(void const * argument)

{

/* USER CODE BEGIN waveformProccess */

uint16_t i,j,k;

osEvent tenCycle;

uint16_t buffAddr,waveSample;

uint8_t hBuff[4480];

uint8_t cylceNum;

int32_t waveBuff[256];

float32_t fftRes[256];

char uartBuff[20];

waveformInfo *waveInfo= (waveformInfo *)osMailAlloc(waveToUarthandle,100);

/* Infinite loop */

for(;;)

{

tenCycle=osSignalWait(BIT_0,200); // waits for recieveing waveform ten cycle samples.

if(tenCycle.status == osEventSignal)

{

for(i=0;i<4480;i++)

hBuff[i]=hBuff_t[i];

for(i=0 ; i <160 ; i++){

waveBuff[160*cylceNum+i]=(uint32_t)(hBuff[28*i+4] << 24 ) | (uint32_t)(hBuff[28*i+5] << 16 ) | (uint32_t)(hBuff[28*i+6] << 8 ) | (uint32_t)(hBuff[28*i+7]);  //   

waveInfo->waveform[i]=waveBuff[i];

}

cylceNum++;

// Take FFT of one cycle of waveform

if(cylceNum==1)

{

osMailFree(waveToUarthandle,waveInfo);

waveformInfo *waveInfo= (waveformInfo *)osMailAlloc(waveToUarthandle,100);

for(i=160;i<256;i++)

{

waveBuff[i]=0;

waveInfo->waveform[i]=waveBuff[i];

}

waveform

FFT

((float32_t *)waveBuff,fftRes,256);

cylceNum = 0;

for(i=0;i<256;i++)

{

waveInfo->waveFFT[i]=fftRes[i];

}

osMailPut(waveToUarthandle,waveInfo); //  sends fft input and output to uart task using mail.

}

}

}

/* USER CODE END waveformProccess */

}

Thanks.

#cmsis-dsp #fft-stm32f4 #freertos
This topic has been closed for replies.

2 replies

Zt Liu
Senior III
November 30, 2017
Posted on November 30, 2017 at 09:12

uint16_t buffAddr,waveSample;

uint8_t hBuff[4480];

uint8_t cylceNum;

int32_t waveBuff[256];

float32_t fftRes[256];

char uartBuff[20]; 

Oh boy! You need lots of heap memory for this task!

Mohammad Hossein
Associate II
November 30, 2017
Posted on November 30, 2017 at 10:21

No problem, I have sufficient  heap. This task needs less than 2000 words. My total heap is about 25000 words.