Skip to main content
AGraj
Visitor II
February 18, 2019
Question

Problem with CAN on STM32F091 uC

  • February 18, 2019
  • 0 replies
  • 561 views

Dear all,

I'm currently trying to work around the CAN Bus on the STM32F091CB uC, with StdPeriph_Lib_V1.5.0 Lib but the transmission is never successful (I have already programmed STM32F4 and STM32F7 boards with StdPeriph_Libs, without any problem).

  1. The concern that has given me is directly the library specifically the file stm32f0xx_can.c, in the @brief says This file provides firmware functions to manage the following  functionalities of the Controller area network (CAN) peripheral and applicable only for STM32F072 devices, that is to say that can't use the CAN Bus Library with my uC ?.
  2. Anyway, I continued to do the code for the CAN peripheral and I find another unknown in the given examples for CAN Bus Peripheral /* CAN Baudrate = 1MBps (CAN clocked at 36 MHz) */, I have calculated an endless number of times with an oscillator HSE = 8MHz, but the result is the same the CAN is clocked a 48MHz. At the end, it's something specific to the HW or a particular thing in the the stm32f0xx_can.c, I don't know ?.

This is my code:

#define CAN_RX_Pin GPIO_Pin_8
 #define CAN_RX_Src GPIO_PinSource8
 #define CAN_RX_Port GPIOB
 
 #define CAN_TX_Pin GPIO_Pin_9
 #define CAN_TX_Src GPIO_PinSource9
 #define CAN_TX_Port GPIOB
 
 #define CAN_AF_Port GPIO_AF_4
 
 void init_CAN_Bus(void){
 	en_CAN_CLK();
 	init_CAN_GPIO();
 	init_CAN_Periph();
 }
 void en_CAN_CLK(void){
 	//Enable GPIOB Src Clk
 	RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE);
 	
 	//Enable CAN Periph Src Clk
 	RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN, ENABLE);
 }
 
 void init_CAN_GPIO(void){
 	// Connect CAN pins to Altinative Funtion 4
 	GPIO_PinAFConfig(CAN_RX_Port, CAN_RX_Src, CAN_AF_Port);
 	GPIO_PinAFConfig(CAN_TX_Port, CAN_TX_Src, CAN_AF_Port);
 
 	//Configure CAN RX & TX pins
 	GPIO_InitTypeDef GPIO_InitStructure;
 	GPIO_StructInit(&GPIO_InitStructure);
 	GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
 	GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
 	GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
 	GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
 
 	GPIO_InitStructure.GPIO_Pin = CAN_RX_Pin;
 	GPIO_Init(CAN_RX_Port, &GPIO_InitStructure);
 
 	GPIO_InitStructure.GPIO_Pin = CAN_TX_Pin;
 	GPIO_Init(CAN_TX_Port, &GPIO_InitStructure);
 }
 
 void init_CAN_Periph(void){
 	//Deinit CAN Periph
 	CAN_DeInit(CAN);
 
 	//Init CAN Periph
 	CAN_InitTypeDef CAN_InitStructure;
 	CAN_StructInit(&CAN_InitStructure);
 	CAN_InitStructure.CAN_TTCM = DISABLE;
 	CAN_InitStructure.CAN_ABOM = DISABLE;
 	CAN_InitStructure.CAN_AWUM = DISABLE;
 	CAN_InitStructure.CAN_NART = DISABLE;
 	CAN_InitStructure.CAN_RFLM = DISABLE;
 	CAN_InitStructure.CAN_TXFP = DISABLE;
 	CAN_InitStructure.CAN_Mode = CAN_Mode_Normal;
 
 	//CAN Baudrate = 500Kbps (CAN clocked at 48 MHz)
 	CAN_InitStructure.CAN_SJW = CAN_SJW_1tq;
 	CAN_InitStructure.CAN_BS1 = CAN_BS1_13tq; //Seg1
 	CAN_InitStructure.CAN_BS2 = CAN_BS2_2tq; //Seg2
 	CAN_InitStructure.CAN_Prescaler = 6; //Prescaler
 	CAN_Init(CAN, &CAN_InitStructure);
 
 	//CAN Filter Init
 	CAN_FilterInitTypeDef CAN_FilterInitStructure;
 	CAN_FilterInitStructure.CAN_FilterNumber = 0;
 	CAN_FilterInitStructure.CAN_FilterMode = CAN_FilterMode_IdMask;
 	CAN_FilterInitStructure.CAN_FilterScale = CAN_FilterScale_32bit;
 	CAN_FilterInitStructure.CAN_FilterIdHigh = 0x0000;
 	CAN_FilterInitStructure.CAN_FilterIdLow = 0x0000;
 	CAN_FilterInitStructure.CAN_FilterMaskIdHigh = 0x0000;
 	CAN_FilterInitStructure.CAN_FilterMaskIdLow = 0x0000;
 	CAN_FilterInitStructure.CAN_FilterFIFOAssignment = 0;
 	CAN_FilterInitStructure.CAN_FilterActivation = ENABLE;
 	CAN_FilterInit(&CAN_FilterInitStructure);
 }

and i transmit with the following function:

uint8_t sndCANBus_Test(void){
 	static CanTxMsg TxMessage;
 
 	TxMessage.StdId = 0x321;
 	TxMessage.ExtId = 0x01;
 	TxMessage.RTR = CAN_RTR_DATA;
 	TxMessage.IDE = CAN_ID_STD;
 
 	TxMessage.Data[0]=0x01;
 	TxMessage.Data[1]=0x02;
 	TxMessage.Data[2]=0x03;
 	TxMessage.Data[3]=0x04;
 	TxMessage.Data[4]=0x05;
 	TxMessage.Data[5]=0x06;
 	TxMessage.Data[6]=0x07;
 	TxMessage.Data[7]=0x08;
 
 	TxMessage.DLC = sizeof(TxMessage.Data);
 
 	uint8_t aux_status;
 	aux_status = CAN_Transmit(CAN, &TxMessage);
 
 	return aux_status;
 }

In the past, the configuration shown above worked for me.

I would be very grateful to all of you for any information that leads me to the solution of this problem, that is, to transmit data to the CAN Bus.

thanks in advance.

This topic has been closed for replies.