Skip to main content
FrankNatoli
Associate III
Apr 1, 2022 4:52 PM UTC
Solved

Problem using dfu-util with STM32H7B3I EVAL board

dfu-util is an open source DFU memory reader/writer.

I ported the source to Windows 10 x64.

Worked fine, downloading firmware, to STM32H7B3I DISCOVERY board.

Fails with STM32H7B3I EVAL board, apparently because the EVAL board identifies itself as three separate DFU devices, unfortunately with identical serial numbers:

Found DFU: [0483:df11] ver=0200, devnum=62, cfg=1, intf=0, path="1-6", alt=2, name="@OTP Memory  /0x1FF7000/01*1024 e", serial="FFFFFFFEFFFF"

Found DFU: [0483:df11] ver=0200, devnum=62, cfg=1, intf=0, path="1-6", alt=1, name="@Option Bytes  /0x1FF8000/01*128 e", serial="FFFFFFFEFFFF"

Found DFU: [0483:df11] ver=0200, devnum=62, cfg=1, intf=0, path="1-6", alt=0, name="@Internal Flash  /0x08000000/256*02Kg", serial="FFFFFFFEFFFF"

Any easy way to resolve this with dfu-util?

Or do I need to "educate" dfu-util in the matter of "alt", which varies with memory region?

This topic has been closed for replies.
MM..1
MM..1Best answer
Super User
Apr 2, 2022 11:02 AM UTC

Why you need dfu-util ? Normal way is STM32_Programmer_CLI.exe -c port=usb1

7 replies

MM..1
Super User
Apr 1, 2022 8:24 PM UTC

Man page

-a, --alt ALT

Specify the altsetting of the DFU interface by name or by number.

FrankNatoli
Associate III
Apr 1, 2022 8:38 PM UTC

Many thanks, that satisfied dfu-util's problem with the three DFU devices.

I inserted --alt 0, because it is the EVAL internal flash that I want to burn, and now dfu-util is complaining "Only DfuSe file version 1.1a is supported", see below.

Probably not coincidentally, dfu-util is reporting "DFU mode device DFU version 011a".

Is dfu-util confused about "1.1a" versus "011a"?

C:\Users\natoli\9500\dfu-util-master\x64\dfu-util\Release>dfu-util --device 0483:df11 --alt 0 -D 9500-Main-USB.out

dfu-util 0.9-msvc

Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.

Copyright 2010-2016 Tormod Volden and Stefan Schmidt

This program is Free Software and has ABSOLUTELY NO WARRANTY

Please report bugs to http://sourceforge.net/p/dfu-util/tickets/

Invalid DFU suffix signature

A valid DFU suffix will be required in a future dfu-util release!!!

Opening DFU capable USB device...

ID 0483:df11

Run-time device DFU version 011a

Claiming USB DFU Interface...

Setting Alternate Setting #0 ...

Determining device status: state = dfuIDLE, status = 0

dfuIDLE, continuing

DFU mode device DFU version 011a

Device returned transfer size 1024

DfuSe interface name: "Internal Flash  "

Only DfuSe file version 1.1a is supported

(for raw binary download, use the --dfuse-address option)

C:\Users\natoli\9500\dfu-util-master\x64\dfu-util\Release>

MM..1
Super User
Apr 2, 2022 3:47 PM UTC
And if you need util seems your file 9500-Main-USB.out isnt compatible format.
MM..1
MM..1Best answer
Super User
Apr 2, 2022 11:02 AM UTC

Why you need dfu-util ? Normal way is STM32_Programmer_CLI.exe -c port=usb1

FrankNatoli
Associate III
Apr 4, 2022 2:05 PM UTC

Friday, STM32CubeProgrammer recognized but was unable to connect to the STM32H7B3I EVAL board.

This morning, it can, cannot explain it.

The rationale behind dfu-util was to use an open source product.