Skip to main content
herbert
Associate III
Aug 7, 2024 9:47 AM UTC
Solved

Problem on STM32F407 and 411 Discovery boards with TIM_CHANNEL_ALL

Hello all,

it seems that when starting a timer in PWM mode, using TIM_CHANNEL_ALL does not work. Everything works fine as long as I start the channels consecutively, (i.e. TIM_CHANNEL_1, then TIM_CHANNEL_2, etc.) but as soon as I change this to TIM_CHANNEL_ALL, the PWM output stops working. Has anyone else encountered this problem yet or am I doing something wrong?

regards
Herby

This topic has been closed for replies.
TDK
TDKBest answer
Aug 7, 2024 11:59 AM UTC

You're calling HAL_TIM_PWM_Start with TIM_CHANNEL_ALL?

TIM_CHANNEL_ALL is not a valid argument for HAL_TIM_PWM_Start, per the source code. They need to be started one at a time.

/**
 * @brief Starts the PWM signal generation.
 * @PAram htim TIM handle
 * @PAram Channel TIM Channels to be enabled
 * This parameter can be one of the following values:
 * @arg TIM_CHANNEL_1: TIM Channel 1 selected
 * @arg TIM_CHANNEL_2: TIM Channel 2 selected
 * @arg TIM_CHANNEL_3: TIM Channel 3 selected
 * @arg TIM_CHANNEL_4: TIM Channel 4 selected
 * @arg TIM_CHANNEL_5: TIM Channel 5 selected
 * @arg TIM_CHANNEL_6: TIM Channel 6 selected
 * @retval HAL status
 */
HAL_StatusTypeDef HAL_TIM_PWM_Start(TIM_HandleTypeDef *htim, uint32_t Channel)
{

 

"If you feel a post has answered your question, please click ""Accept as Solution""."

3 replies

TDK
TDKBest answer
Aug 7, 2024 11:59 AM UTC

You're calling HAL_TIM_PWM_Start with TIM_CHANNEL_ALL?

TIM_CHANNEL_ALL is not a valid argument for HAL_TIM_PWM_Start, per the source code. They need to be started one at a time.

/**
 * @brief Starts the PWM signal generation.
 * @PAram htim TIM handle
 * @PAram Channel TIM Channels to be enabled
 * This parameter can be one of the following values:
 * @arg TIM_CHANNEL_1: TIM Channel 1 selected
 * @arg TIM_CHANNEL_2: TIM Channel 2 selected
 * @arg TIM_CHANNEL_3: TIM Channel 3 selected
 * @arg TIM_CHANNEL_4: TIM Channel 4 selected
 * @arg TIM_CHANNEL_5: TIM Channel 5 selected
 * @arg TIM_CHANNEL_6: TIM Channel 6 selected
 * @retval HAL status
 */
HAL_StatusTypeDef HAL_TIM_PWM_Start(TIM_HandleTypeDef *htim, uint32_t Channel)
{

 

"If you feel a post has answered your question, please click ""Accept as Solution""."
herbert
herbertAuthor
Associate III
Aug 7, 2024 12:10 PM UTC

Thank you, I was wrongly (read carelessly) assuming this works, being lured into the belief by the naming. A closer look into the HAL manual would have revealed the truth ...:face_with_rolling_eyes:

Herbert

TDK
Aug 7, 2024 12:52 PM UTC

The assert_param would also not be passing here. IF you've implemented USE_FULL_ASSERT, this would have been caught within the error handler. (If it's not implemented it just silently fails.)

"If you feel a post has answered your question, please click ""Accept as Solution""."