Skip to main content
elKarro
Associate III
Apr 18, 2025 1:24 PM UTC
Question

possible inconsistency between the RM and the handling of DMA by HAL

ref. RM0440 Rev 9 vs STM32G4xx HAL v1.2.5.0 (en.stm32cubeg4-v1-6-1.zip)

DMA_CCRx.EN - Channel enable
This bit is set and cleared by software.
When a channel transfer error occurs, this bit is cleared by hardware.

DMA_CCRx.TCIE - Transfer complete interrupt enable
DMA_CCRx.HTIE - Half transfer interrupt enable
DMA_CCRx.TEIE - Transfer error interrupt enable
This bit is set and cleared by software.
It is not read-only when the channel is enabled (EN = 1).
It must not be written when the channel is enabled (EN = 1).


"it is not read-only" but "it must not be written when the channel is enabled"
unless RM is a cookbook, this is a must, not a suggestion.
This means that if DMA_CCRx.EN == 1, changing the IE bits along with EN = 0 in a single write must be avoided to prevent entering unpredictable states.
Can ST be exhaustive about changing IE bits along with EN in single writes of DMA_CCRx?

Function HAL_DMA_IRQHandler():
disregarding the RM, __HAL_DMA_DISABLE_IT() is called where the condition DMA_CCRx.EN == 1 is plausible,
in the sections Half Transfer Complete Interrupt management and Transfer Complete Interrupt management.

Function HAL_DMA_Abort():
__HAL_DMA_DISABLE_IT() is called before __HAL_DMA_DISABLE().

This topic has been closed for replies.

1 reply

ST Technical Moderator
May 12, 2025 9:16 AM UTC

Hello @elKarro 

Thank you for bringing this issue to our attention.

I reported this internally.

Internal ticket number: 209452 (This is an internal tracking number and is not accessible or usable by customers).

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om