Skip to main content
OHaza.1
Associate III
Nov 17, 2021 9:27 AM UTC
Solved

Porting Azure RTOS examples

Hi, last time I ported an Azure RTOS project there were only a handful of BSPs so I had to do some manual fiddling around to get it running on a nucleo board. Now that there is full support for H7 processors in the 2.0 package I'm wondering what the best steps to move a project over would be.

I imagine I can start a new project in CubeMX and then "import" the ioc file, generate the base project and then copy in the source code - but wondering if there is a cleaner way of doing it.

TIA, Oliver

This topic has been closed for replies.
STM32_ZA
STM32_ZABest answer
ST Employee
Nov 18, 2021 7:57 AM UTC

Hi,

As you said you need to generate a new project for target board/MCU first then :

1-configure the HW IPs (GPIO, System clock, ETH, USB,,..)

2- Enable/Configure the components of Azure RTOS pack

3- Generate project and copy application source code from an existing example into your new project 

1 reply

STM32_ZA
STM32_ZABest answer
ST Employee
Nov 18, 2021 7:57 AM UTC

Hi,

As you said you need to generate a new project for target board/MCU first then :

1-configure the HW IPs (GPIO, System clock, ETH, USB,,..)

2- Enable/Configure the components of Azure RTOS pack

3- Generate project and copy application source code from an existing example into your new project